Deleting flash memory breaks BLE connection on STM32WB50
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-09-07 5:48 AM
I am using a STM32WB50CGU5, when erasing flash memory where my settings are stored, the BLE connection breaks. It happens even if I erase only one page (number 96).
I think the two CPU conflicts doing flash operations, but the datasheet reports:
"The embedded Flash memory is shared between CPU1 and CPU2 on a time sharing basis. A dedicated HW mechanism allows both CPUs to perform Write/Erase operations."
What can I do to fix this problem?
Is it a BLE stack problem?
- Labels:
-
BLE
-
STM32WB series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-10-09 8:17 AM
The Flash memory is a shared resource protected by 2 semaphores. A core must get the 2 semaphores before performing any data accesses.
those accesses are quite time critical as M0+ core running the RF stack has very tight real time constraints.
If the M4 core is performing even a single block erase at the wrong timing, it could disturb the RF stack so much that the BLE connection is lost.
I would recommend you look at the project under C:\STM32Cube_FW_WB_VX.Y.Z\STM32Cube_FW_WB_V1.8.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_RfWithFlash
This example is to demonstrate the capability to erase/write the flash while a Point-to-Point communication using BLE component is active.