cancel
Showing results for 
Search instead for 
Did you mean: 

Custom coprocessor binaries for STM32WB55

metal2oxide
Associate II

Is it possible to write a custom co-processor binaries for CPU2 instead of using the coprocessor binaries from stm

4 REPLIES 4
TDK
Guru

On the STM32WB series? Next time please include the chip number.

CPU2 on the STM32WB is not user writeable.

https://community.st.com/s/question/0D53W0000090pJe/is-it-possible-to-flash-a-custom-application-to-cpu2-m0

If you feel a post has answered your question, please click "Accept as Solution".
Peter BENSCH
ST Employee

Which multi-core system do you mean?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

If you're doing a few $100M in business, and have a deep bench, a lot of things are possible.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
metal2oxide
Associate II

Thanks for your answer. Yes it is STM32WB55. The doubt is I want to write a IEEE 802.15.4 based application for my project. This should be zephyr rtos based. I am not sure whether the 15.4 stack from st is compatible with zephyr