2017-05-03 2:42 AM
Does anyone have any experience with the current consumption when using B-L072Z-LRWAN1 (STM32L072 and LoRa board) with i-cube-lrwan 110?
I can't get the current consumption below below 1.1mA no matter what i try. In lowpower (stop) mode all pins are set as analog, clocks are disabled, debug is off.
- I checked the device going into STOP mode
- Configured all non-connected pins to GPIO_MODE_ANALOG, GPIO_NOPULL
- Configured connected pins (UART, etc.) to GPIO_MODE_OUTPUT_PP, GPIO_NOPULL, and set to zero
I also stopped the debug clock in the ARM:
__HAL_RCC_DBGMCU_CLK_ENABLE( );
HAL_DBGMCU_DisableDBGSleepMode( );
HAL_DBGMCU_DisableDBGStopMode( );
HAL_DBGMCU_DisableDBGStandbyMode( );
Also TCXO is Off.
Still the current consumption is above 1 mA.
Anyone out there that managed to get the current down?
Thanks!
#lora #b-l072z-lrwan1Solved! Go to Solution.
2017-05-22 3:10 AM
I solved my problem in changing the delay: &sharpdefine TCXO_OFF_DELAY 2. Thanks!
2017-05-17 6:51 AM
Hi,
I'm very interesting by the LoRa consumption using B-L072Z, I have the same problem.
I mesured the RF consumption of my LoRa module after adding the jumpers (
)My measure of Tx (38mA) and Rx (11mA) are ok, but in sleep mode my consumption is too big.
For the RF consumption in sleepmode, I find 1,1mA. My mesure of Tx and Rx are good, but in sleepmode my consumption is too big.
Thanks in advance for any help.
Max2017-05-18 1:06 AM
Have the same problem.
I'm using my custom board and the LoRa module same as in B-L072Z.. My current consumption during stop mode is 1.16mA.
So this is not a B-L072Z hardware problem. I suspect there is some bug in the code (I-CUBE-LRWAN) or hardware problem with LoRa murata module.
2017-05-18 9:20 AM
Hello All,
Referring to
, required setup for power consumption measurement is to have:Updates have to be made in hw_conf.h.
Is it the case for you?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-05-18 10:40 AM
LEDs Off? Other things off the GPIO, USART, etc.
>>
I suspect there is some bug in the code (I-CUBE-LRWAN)
Definately several of those...
2017-05-19 2:11 AM
Hi,
I updated my code to deactivate DEBUG, TRACE and SENSOR ENABLED but I have always 1,16mA in sleep mode.
2017-05-19 2:39 AM
I have only LoRa module, SWD connector, 1 LED (controlled through GPIO) and vdd capacitor on test PCB.
Of course I made a test with disabling: sensors, debug, trace. I have tested the code in configuration with no HW activation, no LoRa initialization and going to
HAL_PWR_EnterSLEEPMode(PWR_MAINREGULATOR_ON, PWR_SLEEPENTRY_WFI);
just after start of the program and still have got 1.16mA
2017-05-19 4:05 AM
Hello,
It seems that TCXO is always enabled in you configuration. Please check JP9 setting: it should be in position 1-2 to have TCXO controlled by PA12.
JP3 is the one that allows you to measure IDD_MCU.
I suggest you to refer to
for more details.Please confirm if this helps you to reach the expected consumption.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-05-19 7:13 AM
With this configuration, the consumption in sleepmode seems to be ok but I can't join my gateway whereas with the JP9 in positon 2-3 I can, there is some modification that I should made?
Thanks in advance
2017-05-19 8:32 AM
I made some screen about my terminal windows in debug and trace with the same code but the JP9 in a different postion: