Posted on September 06, 2017 at 08:55I have question regarding to this topic, maybe someone have any clue.I'm using murata module and ICube-LRWAN software as a base.To get more power from coin battery i'm using a circuit with big capacitors to save ...
Posted on May 19, 2017 at 09:39I have only LoRa module, SWD connector, 1 LED (controlled through GPIO) and vdd capacitor on test PCB.Of course I made a test with disabling: sensors, debug, trace. I have tested the code in configuration with no HW ac...
Posted on May 18, 2017 at 10:06Have the same problem.I'm using my custom board and the LoRa module same as in B-L072Z.. My current consumption during stop mode is 1.16mA.So this is not a B-L072Z hardware problem. I suspect there is some bug in the c...