2018-08-28 02:29 AM
Hello,
When running the example code for the B-L072Z-LRWAN1 module STM32CubeExpansion_LRWAN_V1.2.0 i have an extremely high run current. I added some user code running an algorithm which needs some seconds to terminate. The measured current during MCU calculations is 12.15 mA.
When I look into the datasheet of the STM32L072 processor the calculation current should be around 7 mA.
Why do I have this hight consumption and how do I optimize that?
Regards
2019-04-12 02:43 PM
Hi,
How to do you measure current on discovery board? What is the setup required for it?
Thank You,
2019-04-12 04:00 PM