2020-04-17 3:43 AM
I designed new board with STM32WB55CGU6 based on MB1993C (P-NUCLEO-USBDongle). You can see my schematic attached(I uploaded both P-nucleo schematic and my schematic). But I can't connect to my MCU through SWD pins (DIO,CLK,NRST). I use st-link, I can connect to P-nucleo usbdongle with these 3 pins, but I can't connect to my MCU. ST-Link can't find MCU. Unfortunately one of the crystals in my design (which is connected to pins number 23 and 24) has wrong footprint, but at least I should be able to connect to the MCU. does anyone know what is the problem?
Solved! Go to Solution.
2020-04-17 5:08 AM
Make sure you provide a common ground.
The standalone ST-LINK/V2 (authentic) will also need VCC to pin 1.
If the IC is non-responsive need to focus on power and orientation. Check net list for disconnected or misnamed power nets.
2020-04-17 5:08 AM
Make sure you provide a common ground.
The standalone ST-LINK/V2 (authentic) will also need VCC to pin 1.
If the IC is non-responsive need to focus on power and orientation. Check net list for disconnected or misnamed power nets.