cancel
Showing results for 
Search instead for 
Did you mean: 

connect to a bluetooth device from stm32wb

BLiwa.1
Associate II

Hello,

I want connect to a bluetooth device/sensor from stm32wb and configure the device : for example confgure the period that it shoold advertise for.

Is that possible? If yes how ?

3 REPLIES 3

Have you checked out the documentation available?

0693W00000LyuPMQAZ.png 

@BLiwa.1​ "I want connect to a Bluetooth device/sensor from stm32wb"

So you want the STM32WB to be the Central?

https://www.google.com/search?q=stm32wb+central

"and configure the device"

That would be down to the device firmware - are you also implementing that?

Amel NASRI
ST Employee

Hi @BLiwa.1​ ,

Besides to @Andrew Neil​ 's proposal, I suggest you have a look to the Academy content.

From "Academy" tab on the top, go to eLearning Catalog then select "General Purpose Microcontrollers".

STM32 Wireless BLE is what you need to start with.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Remy ISSALYS
ST Employee

Hello,

Many examples of BLE applications are available in STM32CubeWB package:

https://www.st.com/en/embedded-software/stm32cubewb.html

You can look BLE_HeartRate project (Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_HeartRate) which allows to do fast and low advertising, see Adv_Request in app_ble.c file.

Best Regards