cancel
Showing results for 
Search instead for 
Did you mean: 

Command Line Interface to FUS under MS Windows

FOber.3
Associate

I have to programm half a dozen boards with a STM32WB55RG with BLE LLD firmware, therefor FUS has to be updated in advance. After that the application code must be programmed into the chips. I want to automate this with a batch file, so I don't have to enter startadresses and chose files three times per chip.

Computer runs MS Windows 10

Interface is a ST-Link/V2

1 REPLY 1
Remy ISSALYS
ST Employee

Hello,

You can use the command line interface of STM32CubeProgrammer tool, see user manual UM2237 for command details.

Best Regards