2019-09-14 4:37 AM
Apologies if this has been asked before, I did a search and couldn't find it.....
Using STM32CubeIde, I set the project to be the USB dongle P-Nucleo-WB55. Now, trying to flash this and I am told it doesn't have debug capabilities. Shame, but OK, there is the other board (Nucleo-68) with a very similar chip.
I can not find how to change the target from the USB dongle to the other board. Please help.
Thanks
Ian
Solved! Go to Solution.
2019-09-16 6:13 AM
Unfortunately, there's no way to switch at the moment. It's listed under known issues in the release note as:
"• STM32CubeIDE does not support switching from one MCU to another once the project is created."
You will need to create a new project and copy/paste the relevant code.
2019-09-16 6:13 AM
Unfortunately, there's no way to switch at the moment. It's listed under known issues in the release note as:
"• STM32CubeIDE does not support switching from one MCU to another once the project is created."
You will need to create a new project and copy/paste the relevant code.
2019-09-17 12:32 AM
Thanks for the response. I had missed that :(
Shame, as there was a lot of work linking in files from a larger project I am porting across......
2020-03-31 5:30 AM
hello @Markus GIRDLAND @inky ! is it possible to upload a code that I wrote on my own to USB Dongle? As far as I saw only example can be uploaded because they have binaries. And my code has not binaries.
2020-03-31 6:27 AM
Could you explain a bit further about what you're trying to do? You can have the code itself on the USB dongle but are you trying to execute the code to a dongle?