2025-01-09 9:48 AM - edited 2025-01-09 10:08 AM
Hi, I'm developing my custom board using STM32WB09TEF7TR Microcontroller but have a problem during Programming using STM32cubeIDE.
I can access the memory of this microcontroller using STM32CubeProgrammer through SWD protocol.
However, once I try to import my code to the microcontroller using STM32CubeIDE, the importing fails with error message below.
-----------------------------------------------------------------------
Break at address "0x100017d0" with no debug information available, or outside of program code.
Log output file: C:\Users\GGKIM\AppData\Local\Temp\STM32CubeProgrammer_a31344.log
ST-LINK SN : 0037002F3532510631333430
ST-LINK FW : V3J15M7B5S1
Board : STLINK-V3SET
Voltage : 3.30V
Error: ST-LINK error (DEV_TARGET_RESET_ERR)
2nd connect tentative with frequency (8MHz)
ST-LINK SN : 0037002F3532510631333430
ST-LINK FW : V3J15M7B5S1
Board : STLINK-V3SET
Voltage : 3.30V
Error: ST-LINK error (DEV_TARGET_RESET_ERR)
Encountered Error when opening C:\ST\STM32CubeIDE_1.17.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.2.0.202409170845\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Shutting down...
Exit.
----------------------------------------------------
Do you have any idea why it happened?
I also checked the option byte of this microcontroller. There is only one option byte, RDP. it was FF which means that anybody can do programing.
In addition, I want to try to import my code using the STM32cubeProgrammer by making a bin file from IDE. However, I don't know the starting address.
Does anybody know the starting address for manually importing a code using cubeProgrammer?
FYI, I can see the memory address from 0x10040000 to 0x100BF800, which means 0x100017d0 is outside of memory.
Solved! Go to Solution.
2025-01-10 8:11 AM
This is the same behavior mentioned on the previous link. The RSTN pin should be linked to the NRST pin of your ST-LINK.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-09 12:28 PM
2025-01-09 6:44 PM - edited 2025-01-09 6:44 PM
Thanks for your reply.
I saw the previous post that mentioned soldering the SB30 pin of the developer board.
However, I'm using ST-LINK V3SET to debug my circuit board.
So, I don't know what pin has the same function as SB30.
Do you have any idea on it?
2025-01-10 4:04 AM
Could you please share the schematics of your board and the connection with your ST-LINK.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-10 7:39 AM - edited 2025-01-10 7:44 AM
This is all I can share. Unfortunately, I'm not suing RST (B5) pin of this microcontroller.
2025-01-10 8:11 AM
This is the same behavior mentioned on the previous link. The RSTN pin should be linked to the NRST pin of your ST-LINK.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-10 1:06 PM
I can try but I cannot understand because it wasn't mandatory when I used the STM32WB55 microcontroller.
2025-01-11 2:43 AM
Thanks. Now IDE is working now by connecting NRST to RST.
2025-01-11 2:56 AM
@KKIM.6 wrote:I cannot understand because it wasn't mandatory when I used the STM32WB55 microcontroller.
Indeed, NRST isn't generally needed, but there are cases where it is necessary - particularly where the application goes to sleep and/or disables the debug pins.
This is why it's always good to include access to NRST in your debug/programming connection.