Cannot load Wireless firmware into STM32WB55 Nucleo board
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-02 4:48 AM
Hi, am using the STM32WB55 Nucleo board. My problem is, currently I
seem not to have a CPU2 wireless stack loaded and I fail to load file
stm32wb5x_BLE_Stack_full_fw.bin loaded into the Flash. I am using the
STM32CubeProgrammer V2.12.0. When selecting on the Firmware Upgrade
Service Button and clicking on "Read FUS infos", I get:
FUS State: FUS_IDLE
FUS Status: FUS_NO_ERROR
FUS Version: v0.0.0.0
FUS Operator: v3.1.0
When I click on "Start Wireless Stack", this happens:
13:20:53 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.
13:20:53 : Warning: Option Byte: nboot0, value: 0x1, was not modified.
13:20:53 : Warning: Option Byte: nboot1, value: 0x1, was not modified.
13:20:53 : Warning: Option Bytes are unchanged, Data won't be downloaded
13:20:53 : Time elapsed during option Bytes configuration: 00:00:00.000
13:20:53 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1
13:20:53 : Memory Programming ...
13:20:53 : Opening and parsing file: 0x495_FUS_Operator.bin
13:20:53 : File : 0x495_FUS_Operator.bin
13:20:53 : Size : 8.00 KB
13:20:53 : Address : 0x08000000
13:20:53 : Erasing memory corresponding to segment 0:
13:20:53 : Erasing internal memory sectors [0 1]
13:20:53 : Download in Progress:
13:20:53 : File download complete
13:20:53 : Time elapsed during download operation: 00:00:00.532
13:20:54 : Application is running, Please Hold on...
13:20:55 : Reconnecting...
13:20:55 : Reconnected !
13:20:55 : Error: FUS_STATE_ERR_UNKNOWN: Unknown error
13:20:55 : Start Wirless Stack failed
13:20:55 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.
13:20:55 : Warning: Option Byte: nboot0, value: 0x1, was not modified.
13:20:55 : Warning: Option Byte: nboot1, value: 0x1, was not modified.
13:20:55 : Warning: Option Bytes are unchanged, Data won't be downloaded
13:20:55 : Time elapsed during option Bytes configuration: 00:00:00.000
13:20:55 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1
13:20:55 : Memory Programming ...
13:20:55 : Opening and parsing file: 0x495_FUS_Operator.bin
13:20:55 : File : 0x495_FUS_Operator.bin
13:20:55 : Size : 8.00 KB
13:20:55 : Address : 0x08000000
13:20:55 : Erasing memory corresponding to segment 0:
13:20:55 : Erasing internal memory sectors [0 1]
13:20:55 : Download in Progress:
13:20:55 : File download complete
13:20:55 : Time elapsed during download operation: 00:00:00.542
13:20:55 : Application is running, Please Hold on...
13:20:56 : Reconnecting...
13:20:56 : Reconnected !
13:20:56 : Error: FUS_STATE_ERR_UNKNOWN: Unknown error
13:20:56 : Start Wireless Stack Operation Failure! Please, try again
So it seems, there is no Wireless Stack present. And if I try to load
it, this also fails: I want to use stm32wb5x_BLE_Stack_full_fw.bin
(V1.15). From the release note, I learn that the correct start address
is 0x080CE000. I have the
"First install" checkbox deselected, and the "Verify download"
selected. The Start Address field is set to 0x080CE000. On clicking
"Firmware Upgrade", I get this log:
13:23:58 : Old Firmware delete ...
13:23:58 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.
13:23:58 : Warning: Option Byte: nboot0, value: 0x1, was not modified.
13:23:58 : Warning: Option Byte: nboot1, value: 0x1, was not modified.
13:23:58 : Warning: Option Bytes are unchanged, Data won't be downloaded
13:23:58 : Time elapsed during option Bytes configuration: 00:00:00.001
13:23:58 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1
13:23:58 : Memory Programming ...
13:23:58 : Opening and parsing file: 0x495_FUS_Operator.bin
13:23:58 : File : 0x495_FUS_Operator.bin
13:23:58 : Size : 8.00 KB
13:23:58 : Address : 0x08000000
13:23:58 : Erasing memory corresponding to segment 0:
13:23:58 : Erasing internal memory sectors [0 1]
13:23:58 : Download in Progress:
13:23:59 : File download complete
13:23:59 : Time elapsed during download operation: 00:00:00.532
13:23:59 : Application is running, Please Hold on...
13:24:06 : Reconnecting...
13:24:06 : Reconnected !
13:24:06 : Warning: FUS_STATE_ERR_UNKNOWN
And when trying to start the firmware, I still get 2 dialog boxes
"Error: FUS_STATE_ERR_UNKNOWN error", and the log window shows:
13:26:37 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.
13:26:37 : Warning: Option Byte: nboot0, value: 0x1, was not modified.
13:26:37 : Warning: Option Byte: nboot1, value: 0x1, was not modified.
13:26:37 : Warning: Option Bytes are unchanged, Data won't be downloaded
13:26:37 : Time elapsed during option Bytes configuration: 00:00:00.000
13:26:37 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1
13:26:37 : Memory Programming ...
13:26:37 : Opening and parsing file: 0x495_FUS_Operator.bin
13:26:37 : File : 0x495_FUS_Operator.bin
13:26:37 : Size : 8.00 KB
13:26:37 : Address : 0x08000000
13:26:37 : Erasing memory corresponding to segment 0:
13:26:37 : Erasing internal memory sectors [0 1]
13:26:37 : Download in Progress:
13:26:38 : File download complete
13:26:38 : Time elapsed during download operation: 00:00:00.533
13:26:38 : Application is running, Please Hold on...
13:26:39 : Reconnecting...
13:26:39 : Reconnected !
13:26:39 : Error: FUS_STATE_ERR_UNKNOWN: Unknown error
13:26:39 : Start Wirless Stack failed
13:26:39 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.
13:26:39 : Warning: Option Byte: nboot0, value: 0x1, was not modified.
13:26:39 : Warning: Option Byte: nboot1, value: 0x1, was not modified.
13:26:39 : Warning: Option Bytes are unchanged, Data won't be downloaded
13:26:39 : Time elapsed during option Bytes configuration: 00:00:00.001
13:26:39 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1
13:26:39 : Memory Programming ...
13:26:39 : Opening and parsing file: 0x495_FUS_Operator.bin
13:26:39 : File : 0x495_FUS_Operator.bin
13:26:39 : Size : 8.00 KB
13:26:39 : Address : 0x08000000
13:26:39 : Erasing memory corresponding to segment 0:
13:26:39 : Erasing internal memory sectors [0 1]
13:26:39 : Download in Progress:
13:26:39 : File download complete
13:26:39 : Time elapsed during download operation: 00:00:00.534
13:26:39 : Application is running, Please Hold on...
13:26:40 : Reconnecting...
13:26:40 : Reconnected !
13:26:40 : Error: FUS_STATE_ERR_UNKNOWN: Unknown error
13:26:40 : Start Wireless Stack Operation Failure! Please, try again
I have found some similar questions:
- Issue: Attempting to flash firmware onto coprocessor on STM32WB55RGV6
results in Error: FUS_STATE_ERR_UNKNOWN
- [STM32WB55 Nucleo] Unable to update FUS or the wireless stack
(FUS_STATE_ERR_UNKNOWN)
but both threads do not seem to have a solution.
I also read the AN5185 as well as the STM32WB_FUS wiki I am not allowed to post a link here, so I will split it:
"stm32mcu/wiki/Connectivity:STM32WB_FUS"
on
but to no avail.
I tried to identify the FUS version. IPCCDBA option byte is 0, but the whole
memory starting at 02x0030000 contains only 0x000000, so I don't find
the Device info table.
The SBRV option bytes contain 0x3d800, so this seems to indicate I
have FUS V0.5.3 loaded.
These seem to be the relevant option bytes on my board:
RDP: 0xAA (nor read protection)
nBOOT0: 1
nBOOT1: 1
ESE: unchecked
SFSA: 0xd4
FSD, DDS, C2OPT, NBRSD: checked
SNBRSA: 0x13
BRSD: checked
SBRSA: 0x0a
SBRV: 0x3d800
Any help would by nice!
Regards
Dirk
- Labels:
-
BLE
-
STM32WB series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-02 7:02 AM
On left side release html info is step by step howto update. Primary first need update FUS.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-02 7:50 AM
The problem is, that step 4 of that instruction does not work, i.e. I have no reliable information about the current FUS version (0.0.0.0 is not mentioned as possible value). I only assume it is 0.5.3 from the SBRV value, but I am not sure. And I don't want to brick my board.
[D:\work]STM32_Programmer_CLI.exe -c port=swd -startfus
-------------------------------------------------------------------
STM32CubeProgrammer v2.12.0
-------------------------------------------------------------------
ST-LINK SN : 066FFF545057717867055444
ST-LINK FW : V2J40M27
Board : P-NUCLEO-WB55
Voltage : 3.26V
SWD freq : 4000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x495
Revision ID : Rev B
Device name : STM32WB5x/35xx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0xD2
Debug in Low Power mode enabled
Warning: Option Byte: nSWboot0, value: 0x0, was not modified.
Warning: Option Byte: nboot0, value: 0x1, was not modified.
Warning: Option Byte: nboot1, value: 0x1, was not modified.
Warning: Option Bytes are unchanged, Data won't be downloaded
Time elapsed during option Bytes configuration: 00:00:00.007
Succeeded to set nSWboot0=0 nboot1=1 nboot0=1
Memory Programming ...
Opening and parsing file: 0x495_FUS_Operator.bin
File : 0x495_FUS_Operator.bin
Size : 8.00 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 1]
Download in Progress:
██████████████████████████████████████████████████ 100%
File download complete
Time elapsed during download operation: 00:00:00.580
Application is running, Please Hold on...
Reconnecting...
Reconnected !
Reconnecting...
Reconnected !
StartFus activated successfully
FUS_STATE_IDLE
startfus command execution finished
[D:\work]STM32_Programmer_CLI.exe -c port=swd mode=UR -r32 0x20030030 1
-------------------------------------------------------------------
STM32CubeProgrammer v2.12.0
-------------------------------------------------------------------
ST-LINK SN : 066FFF545057717867055444
ST-LINK FW : V2J40M27
Board : P-NUCLEO-WB55
Voltage : 3.26V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x495
Revision ID : Rev B
Device name : STM32WB5x/35xx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0xD2
Debug in Low Power mode enabled
Reading 32-bit memory content
Size : 4 Bytes
Address: : 0x20030030
0x20030030 : 00000000
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-02 8:46 AM
Use GUI Programmer not cli
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-02 8:51 AM
Just the same problem, see above: "FUS Version: v0.0.0.0"
And reading from 0x2003000 on gives ony 0x000000 for the whole range.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-02 8:53 AM
Send PM teamviewer
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-02 9:50 AM
If you dont sucess maybe this help Unable to start FUS
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-02 10:01 AM
Had no success, could not update the FUS (ended up with "FUS_STATE_ERR_UNKNOWN). But your reference looks promising, at least the symptoms look very similar to the observed ones. Once again thank you for your help!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-08 11:30 AM
I have same issue, but with STM32WB15. Today I was updating it to 1.16 and got the same symptoms, option bytes are slightly different:
SBRV: 0x8400
SFSA: 0x31
When I click on read FUS infos, sometimes it shows FUS Version v23.ffffffa8.7d.ffffffef, but 99% of the time it shows 0.0.0.0. Start FUS always gives an error.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-08 12:46 PM
Try slow down stlink speed from 4M to 400kHz or less