2021-01-18 10:04 AM
Hello,
I am using STM32 Cube Ide and I am just getting started with the STM32 WB55 board. I tried running the p2p Server project from the firmware package but I can't see the board neither on nrf Connect application or ST BLE Sensor app. Does anyone has the same problem ?
2021-01-22 06:26 AM
Did you try to load the BLE_p2pServer_reference.hex file located under the
STM32Cube_FW_WB_V1.10.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_p2pServer\Binary directory.
Then use the ST BLE sensor mobile application to detect it and connect to it.
This would ensure your board is OK.