2023-05-17 10:33 PM
2023-05-17 11:28 PM
Isn't that the part Murata uses in the LRWAN1 DISCOVERY ??
2023-05-18 2:10 AM - edited 2023-11-20 5:09 AM
read in manual...
https://www.st.com/en/embedded-software/i-cube-lrwan.html
2023-05-18 8:29 AM
Any STM32 can be used for LoRA, they tend to focus on the Low Power ones because that's where the squeaky wheels are, but I've built / ported the LRWAN (Semtech) code onto F4 and F7 platforms, among others, to support LoRa P2P in applications where I want to avoid adding additional legs of latency and UART links, etc.