cancel
Showing results for 
Search instead for 
Did you mean: 

Can I receiev ADC char from Board STM32WB55 to the USB Dongle or android application

MKolo.2
Associate II

Hello,

Can anyone help me on how to receive characters from STM32WB55 to the USB DONGLE as a receiver to show the ADC values.

Or send the values via BLE Gatt to an android application using the inbuilt BLE services in STM32WB55.

The material offered are too shallow especially the USB Dongle.

Thank you.

Regards,

M.E

6 REPLIES 6
MM..1
Chief II

It just send a signal to toggle the led and not sending the individual char. I need to read the individual char in the android application.

12c

Do ypu have any place where I can send ADC values. In which place in the interupt and how can I impliment such a function.

Can you please tell me the file name and the function or add the string "Thanks" to the fuctions. It will be of big help. Thank you in advance.

MKolo.2
Associate II

There is no way anyone can help me get through this problem, I need to finish my project. All material available are for ADRUINO. Why cant we atleast have answers when we need. Any buffer where I can add my message?????