2022-07-19 8:56 AM
Hello,
I would like to reach the lowest consumption as possible. I am programming an end node which sends data through TTN. My project is based on the LoRaWAN End Node example with the LoRaWAN middleware.
My fimrware works like that :
The example PWR_STANDBY works without any problem, I reach a consumption of 1.1 µA. I copied the code that configures and turns the board in standby mode into my firmware but at each boot, after reached the function HAL_PWR_EnterSTANDBYMode(), the board resets automatically.
Do you have any idea what I did wrong or miss in my firmware ? I can add the source code if needed.
I am using a custom board with the LoRa E5 STM32WL5EJC module embedded and the STM32WL package.
Thanks you in advance
Regards
2024-06-16 11:15 PM
Is there a generic solution to this for all of the STM32 Family?
I am currently trying to enter SHUTDOWN Mode in an STM32U083 and the processor keeps resetting and starting to run the code from the beginning again.
I'm calling:
HAL_PWR_EnterSHUTDOWNMode
I have added:
PWR->SCR = PWR_SCR_CWUF; // Clear wakeup flags
To the void HAL_PWR_EnterSHUTDOWNMode(void) function but it is still resetting.