‎2024-02-22 06:16 PM
hello.
As I said in the title, I would like to know the exact Bluetooth version information for both MCUs.
I recognize the Bluetooth version of stm32wb5mmg as '5.0'. However, the datasheet and MCU website say that the Bluetooth version is '5.4'. Which version is correct?
I would also like to know the Bluetooth version information of stm32wb1mmc.
Is there a way to find out the exact Bluetooth version information?
The datasheet is attached, and below is the MCU website I checked.
stm32wb5mmg website:
https://www.st.com/en/microcontrollers-microprocessors/stm32wb5mmg.html
stm32wb1mmc website:
https://www.st.com/en/microcontrollers-microprocessors/stm32wb1mmc.html
Solved! Go to Solution.
‎2024-02-23 12:04 AM
You can change the version of Bluetooth in the CubeMX if i am not wrong. so stm32wb5mmg does support bluetooth version 5.4 and for stm32wb1mmc , It supports bluetooth 5.4 as well. all you need is, when you are doing settings for your project
‎2024-02-23 12:04 AM
You can change the version of Bluetooth in the CubeMX if i am not wrong. so stm32wb5mmg does support bluetooth version 5.4 and for stm32wb1mmc , It supports bluetooth 5.4 as well. all you need is, when you are doing settings for your project
‎2024-02-23 12:19 AM
Hello @KWOOJ
As said @SikandarLF both STM32WB1MMC and STM32WB5MMG support both BLE 5.4. But, you can configure them to use even a lower version for maybe adaptation needs.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
‎2024-02-28 02:39 AM
Hello,
Please don't be confused between Bluetooth version and real Bluetooth features supported.
Every features are optional, meaning you can have a device Bluetooth 5.4 certified but supporting only features of 5.1 for example.
Please refer to Certification guideline for STM32WB and STM32WBA - stm32mcu for having latest certification version of stm32wb5mmg or stm32wb1mmc.
As can be seen here, STM32WB5MMG is having a 5.3 component QDID (187035) and can be combined with a stack version 5.4 (QDID 216169) so this module can be stated as bluetooth 5.4 (again does not mean it supports all 5.4 features)
STM32WB1MMC is having a 5.3 component QDID (187042) and can be combined with a stack version 5.4 (QDID 216169) so this module can be stated as bluetooth 5.4 (here again does not mean it supports all 5.4 features)
Regards
Laurent
‎2024-03-22 12:51 AM
With your help, I have accurate information.
I was able to set the Bluetooth version through CUBEMX.
It helped me solve my problem
thank you