cancel
Showing results for 
Search instead for 
Did you mean: 

Bluetooth classic profiles (SPP / A2DP) on STM32WB

JUker
Associate II

Hello,

I have experience using Bluetooth classic profiles: SPP and A2DP.

Started using STM32WB and I understand it doesn't support these two above profiles, it only has a stack for BLE. Is this correct?

Can I use STM32WB with SPP and/or A2DP, if yes - how? if no - what profiles supported by the STM32WB do you recommend (to replace SPP and A2DP)?

In addition, I've noticed ST has Bluetooth devices of series BlueNRG and SPBTLE: what is the difference between these two and the STM32WB?

Do they support SPP and A2DP

Thanks,

Jig

13 REPLIES 13
EMECH
ST Employee

Serial Port configuration:

0690X00000AA63VQAT.jpg

EMECH
ST Employee

And the Terminal screen:

0690X00000AA61ZQAT.jpg

Best regards.

Same issue , same feeling, one would think propper support and documentation could be done in 2 years but apparently no.

https://community.st.com/s/question/0D53W000013pMSvSAM/blecablereplacement-doesnt-work-for-me-pnucleowb55

we dont need to firmware by ourselves, lets talk
ptagh.1
Associate II

Hello guys,

I wanna implement the BLE_CableReplacement example on the Nucleo board.

But I don't know which application/example should be programmed on Dongle.

I need to have a full-duplex communication between Dongle & Nucleo (Stream of data).