cancel
Showing results for 
Search instead for 
Did you mean: 

BLE - Single peripheral to multiple central connection

DS.4
Senior II

Using the NUCLEO board with STM32WB.

Device is currently configured as server to act as a peripheral. (one of the examples)

I am interested in connecting it to multiple central.

Is it possible?

Any example will be great.

2 REPLIES 2
Remi QUINTIN
ST Employee

You can have a look at the router project. It is an example of a device support up to 6 connections to others peripherals as a central device + 2 others connections as a peripheral to 2 central devices.

Please share the link