cancel
Showing results for 
Search instead for 
Did you mean: 

WB35 BLE application not working

Asperagabriel
Associate II

Here at the university we have some projects using STM32WB for BLE applications, but we only have succeeded after messing around with teh BLE_CUSTOM example and overwriting some info into the ioc via notepad (it was used to be able to change the file name and such thing), and after that we were able to configure the BLE in the  STM32CubeMX normally, but when made from scratch, even following this ST tutorial, the server wouldn't show up neither on the ST BLE Toolbox nor LightBlue apps, but when i use the example it works fine. If i was going to use the STM32WB55 it would be fine, but as we are changing to the STM32WB35, which has no examples avaible on the STM32CubeMX, i have stumbled upon a big trouble making it work. Is there any setting or step that i am probably missing that is not indicated on the tutorial?

Edit: STM32CubeIDE not STM32CubeMX*

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0