2020-04-21 11:42 PM
Hello,
I am trying to develop app based on BLE_MeshLightingProvisioner example.
From the readme file, I know that the node can be self provisioned and configured when the ENABLE_PROVISIONER_FEATURE is defined. This is a great feature and I want to use it.
So I uncommented ENABLE_PROVISIONER_FEATURE define.
In this example, there is a problem with FLASH access. As can you see on the screenshot AppliPrvnNvm_Process tries to save data but it is always HAL_TIMEOUT.
After more tests I can see when microcontroller is fully cleared (RDP -> 0xBB -> 0xAA) this function works properly and returns HAL_OK.
But after reset there is always HAL_TIMEOUT returned.
The next problem with FLASH access is that I can not write my data to FLASH.
In the cube version 1.6.0 there is provided an example BLE_RfWithFlash with flash_driver.c.
The new flash driver should provide correct synchronization between the two cores during flash access.
I made the following changes based on this example.
Inside my mesh app I change MoblePalNvmWrite and MoblePalNvmErase using functions from flash_driver.c. Please look at the code below.
MOBLE_RESULT MoblePalNvmErase(MOBLEUINT32 address,
MOBLEUINT32 offset)
{
HAL_StatusTypeDef status = HAL_OK;
FLASH_EraseInitTypeDef erase;
erase.TypeErase = FLASH_TYPEERASE_PAGES;
erase.Page = GetPage(address + offset); /* 126 or 127 */;
erase.NbPages = FLASH_SECTOR_SIZE >> 12;
FD_EraseSectors(erase.Page, erase.NbPages);
return status == HAL_OK ? MOBLE_RESULT_SUCCESS : MOBLE_RESULT_FAIL;
}
MOBLE_RESULT MoblePalNvmWrite(MOBLEUINT32 address,
MOBLEUINT32 offset,
void const *buf,
MOBLEUINT32 size)
{
MOBLE_RESULT result = MOBLE_RESULT_SUCCESS;
if (offset > NVM_SIZE)
{
result = MOBLE_RESULT_INVALIDARG;
}
else if (size == 0)
{
result = MOBLE_RESULT_FALSE;
}
else if (offset + size > NVM_SIZE)
{
result = MOBLE_RESULT_INVALIDARG;
}
else if (offset & 3)
{
result = MOBLE_RESULT_INVALIDARG;
}
else if (size & 3)
{
result = MOBLE_RESULT_INVALIDARG;
}
else
{
size >>= 3;
uint64_t* src = (uint64_t*)buf;
for (size_t i = 0; i < size; i++)
{
do
{
FD_WriteSingleData(address + offset + (i <<3), src[i]);
} while(*((uint64_t*)(address + offset + (i <<3))) != src[i]);
}
}
return result;
}
I also call SHCI_C2_SetFlashActivityControl(FLASH_ACTIVITY_CONTROL_SEM7); at the end of void APP_BLE_Init( void );
There is more changes in stm32wbxx_it.c connected with using semaphores.
I also copied these wrap function to my project:
/* USER CODE BEGIN FD_WRAP_FUNCTIONS */
#if(CFG_USE_SEQ_TO_WAIT_FOR_SEM == 1)
WaitedSemStatus_t FD_WaitForSemAvailable(WaitedSemId_t WaitedSemId)
{
if(WaitedSemId == WAIT_FOR_SEM_BLOCK_FLASH_REQ_BY_CPU1)
{
LL_HSEM_ClearFlag_C1ICR(HSEM, __HAL_HSEM_SEMID_TO_MASK(CFG_HW_BLOCK_FLASH_REQ_BY_CPU1_SEMID)); /* There is a bug in __HAL_HSEM_CLEAR_FLAG() */
if(LL_HSEM_GetStatus(HSEM, CFG_HW_BLOCK_FLASH_REQ_BY_CPU1_SEMID))
{
APP_DBG_MSG("\r\n\rWAIT UNTILL CPU1 ALLOWS FLASH OPERATION\n");
HAL_HSEM_ActivateNotification(__HAL_HSEM_SEMID_TO_MASK(CFG_HW_BLOCK_FLASH_REQ_BY_CPU1_SEMID));
UTIL_SEQ_WaitEvt( 1<< CFG_IDLEEVT_FLASH_OPER_ALLOWED);
HAL_HSEM_DeactivateNotification(__HAL_HSEM_SEMID_TO_MASK(CFG_HW_BLOCK_FLASH_REQ_BY_CPU1_SEMID));
}
}
if(WaitedSemId == WAIT_FOR_SEM_BLOCK_FLASH_REQ_BY_CPU2)
{
LL_HSEM_ClearFlag_C1ICR(HSEM, __HAL_HSEM_SEMID_TO_MASK(CFG_HW_BLOCK_FLASH_REQ_BY_CPU2_SEMID)); /* There is a bug in __HAL_HSEM_CLEAR_FLAG() */
if(LL_HSEM_GetStatus(HSEM, CFG_HW_BLOCK_FLASH_REQ_BY_CPU2_SEMID))
{
APP_DBG_MSG("\r\n\rWAIT UNTILL CPU2 ALLOWS FLASH OPERATION\n");
HAL_HSEM_ActivateNotification(__HAL_HSEM_SEMID_TO_MASK(CFG_HW_BLOCK_FLASH_REQ_BY_CPU2_SEMID));
UTIL_SEQ_WaitEvt( 1<< CFG_IDLEEVT_FLASH_OPER_ALLOWED);
HAL_HSEM_DeactivateNotification(__HAL_HSEM_SEMID_TO_MASK(CFG_HW_BLOCK_FLASH_REQ_BY_CPU2_SEMID));
}
}
return WAITED_SEM_FREE;
}
#endif
void HAL_HSEM_FreeCallback(uint32_t SemMask)
{
if(SemMask == __HAL_HSEM_SEMID_TO_MASK(CFG_HW_BLOCK_FLASH_REQ_BY_CPU1_SEMID))
{
UTIL_SEQ_SetEvt(1<< CFG_IDLEEVT_FLASH_OPER_ALLOWED);
}
if(SemMask == __HAL_HSEM_SEMID_TO_MASK(CFG_HW_BLOCK_FLASH_REQ_BY_CPU2_SEMID))
{
UTIL_SEQ_SetEvt(1<< CFG_IDLEEVT_FLASH_OPER_ALLOWED);
}
}
void HAL_MspInit(void)
{
/* USER CODE BEGIN MspInit 0 */
/* USER CODE END MspInit 0 */
__HAL_RCC_HSEM_CLK_ENABLE();
/* System interrupt init*/
/* USER CODE BEGIN MspInit 1 */
/* HSEM_IRQn interrupt configuration */
HAL_NVIC_SetPriority(HSEM_IRQn, 15, 0);
HAL_NVIC_EnableIRQ(HSEM_IRQn);
/* USER CODE END MspInit 1 */
}
/* USER CODE END FD_WRAP_FUNCTIONS */
On the screenshot you can see endless execution do {} while() because of flash write fails.
From this forum I know that there are problems with FLASH access in examples based on BLE. But in mesh write to FLASH does not work at all.
Anyone plays with BLE mesh and deal with this issue?
2020-04-28 1:48 AM
Hello,
You cannot set the 2 features ENABLE_PROVISIONER_FEATURE and DYNAMIC_PROVISIONER at the same time.
Perhaps it is not clearly explained in the readme.txt file.
It seems that with the ENABLE_PROVISIONER_FEATURE, some FLASH trouble access happens after each reset of the board, this trouble will be solved in the next releasee.
Nevertheless the BLE_MeshLightingProvisioner project is an example of embedded provisioner, the default configuration settings of this project is the Dynamic provisioner.
In this configuration the FLASH accesses works.
The Dynamic provisioner feature is not so different than the provisioner feature, the diffference is that after initialization the device is seen as an unprovisioned device.
To become self provisioned and self configured, you have to open an external terminal with the following configuration:
First unprovision the device:
And run the following command:
atep root
To be sure that the device is correctly provisioned and configured, just press SW1 button, if the blue LED is on it is OK, if not unprovisions the device and run again the command atep root.
For a scan of the unprovisioned devices, run the command:
atep scan
UUID addresses of the unporvisioned devices are displayed as following:
Device-0 -> F81D4FAE7DEC4B53A154F6FB0726E1C0
To provision and configure the device run the command:
atep prvn-0 2
Where:
Parameter 0 is the displayed index of the device
Parameter 2 is the unicast address you want to associates to the provisioned node (1 is used for the provisioner Node)
After running this command, many lines are displayed on the terminal, till the following one:
38281 Appli_ConfigClient_ConfigureNode - **Node is configured**.
For any other questions, do not hesitate.
Best regards.
2020-04-28 2:18 AM
Hello,
thank you for the answer.
I set only ENABLE_PROVISIONER_FEATURE so I did this right.
I want to use ENABLE_PROVISIONER_FEATURE because I will not have direct access to the final device. Self-provisioning and self-configuration will save a lot of time in my installation. The only thing is the unicast address should be different for each device. I want to use the serial number to generate the address and send it in the broadcast to the concentrator.
I will check the Dynamic provisioner feature maybe this will be better than configuration from the smartphone.
What about flash_driver.c provided in BLE_RfWithFlash example?
It will be included in Mesh example? Because I have trouble with store my own data/setting in FLASH.
Best Regards
2020-04-29 5:29 AM
Hello EMECH,
I play with Dynamic Provisioner. Below is the log from my attempts. Can you tell me what am I doing wrong, Because I can not provision any device?
Next NVM Address 080c703c
Provisioned node
Provisioned Node Address: [0001]
********************
PB-ADV Enabled
PB-GATT Enabled
Feature: Relay Enabled
Feature: Proxy Enabled
Feature: Friend Enabled
Models data will be saved in Flash
Embedded Provisioner data saving enabled
Number of Elements enabled: 1
Neighbour Table is enabled
Generic On Off Server Model enabled
********************
BLE-Mesh Lighting Demo v1.12.007
BLE-Mesh Library v01.12.007
BLE Stack v1.6.0 Branch=0 Type=3
FUS v1.1.0
BD_MAC Address = [c0]:[e1]:[26]:[07]:[be]:[d2]
UUID Address = [f8] [1d] [4f] [ae] [7d] [ec] [4b] [53] [a1] [54] [d2] [be] [07] [26] [e1] [c0]
645 Model_RestoreStates - No Saved Data Found
645 Generic_PowerOnOff_Set - Generic_PowerOnOff_Set callback received
645 GenericModelServer_GetStatusRequestCb - response status enable
Publishing the Power on state to address C000
atep scan
atep scan
Device-0 -> F81D4FAE7DEC4B53A154BA380326E1C0
Device-1 -> F81D4FAE7DEC4B53A154034D0326E1C0
Device-2 -> F81D4FAE7DEC4B53A154DD340326E1C0
Test command executed successfully
atep prvn-0 2
atep prvn-0 2
Test command executed successfully
33996 BLEMesh_PbAdvLinkOpenCb - PB-ADV Link opened successfully
40742 BLEMesh_PvnrDataInputCallback - Device Key: e2 db 93 b1 14 ac 1c 76 ab 41 36 05 d4 1a 37 ca
40742 BLEMesh_PvnrDataInputCallback - App Key: 8c 70 1b 33 f5 14 0f 28 26 70 91 f5 70 83 ee dd
40743 BLEMesh_PvnrDataInputCallback - Node Address Assigned = 0
Device is provisioned by provisioner
52347 BLEMesh_PbAdvLinkCloseCb - PB-ADV Link Closed successfully
52347 AppliPrvnNvm_Process - Saving in SubPage[00000050] =
54353 ConfigClient_CompositionDataGet - Config CompositionDataGet Message
74353 ConfigClient_ChkRetries - Retry started
76353 ConfigClient_CompositionDataGet - Config CompositionDataGet Message
96353 ConfigClient_ChkRetries - Retry started
98353 ConfigClient_CompositionDataGet - Config CompositionDataGet Message
118353 ConfigClient_ErrorState - No response from Node
atep scan
atep scan
Device-0 -> F81D4FAE7DEC4B53A154034D0326E1C0
Device-1 -> F81D4FAE7DEC4B53A154DD340326E1C0
Test command executed successfully
atep scan
atep scan
Device-0 -> F81D4FAE7DEC4B53A154034D0326E1C0
Device-1 -> F81D4FAE7DEC4B53A154DD340326E1C0
Test command executed successfully
atep scan
atep scan
Device-0 -> F81D4FAE7DEC4B53A154034D0326E1C0
Device-1 -> F81D4FAE7DEC4B53A154DD340326E1C0
Test command executed successfully
atep scan
atep scan
Device-0 -> F81D4FAE7DEC4B53A154034D0326E1C0
Device-1 -> F81D4FAE7DEC4B53A154DD340326E1C0
Test command executed successfully
atep scan
atep scan
Device-0 -> F81D4FAE7DEC4B53A154034D0326E1C0
Device-1 -> F81D4FAE7DEC4B53A154DD340326E1C0
Test command executed successfully
atep scan
atep scan
Device-0 -> F81D4FAE7DEC4B53A154034D0326E1C0
Device-1 -> F81D4FAE7DEC4B53A154DD340326E1C0
Test command executed successfully
atep scan
atep scan
Device-0 -> F81D4FAE7DEC4B53A154034D0326E1C0
Device-1 -> F81D4FAE7DEC4B53A154DD340326E1C0
Test command executed successfully
atep scan
atep scan
Device-0 -> F81D4FAE7DEC4B53A154BA380326E1C0
Device-1 -> F81D4FAE7DEC4B53A154034D0326E1C0
Device-2 -> F81D4FAE7DEC4B53A154DD340326E1C0
Test command executed successfully
atep prvn-1 2
atep prvn-1 2
Test command executed successfully
279597 BLEMesh_PbAdvLinkOpenCb - PB-ADV Link opened successfully
289353 BLEMesh_PvnrDataInputCallback - Device Key: 1f 64 ed 5c 17 e3 99 7c 72 97 4a 8e c5 76 f0 05
289354 BLEMesh_PvnrDataInputCallback - App Key: 8c 70 1b 33 f5 14 0f 28 26 70 91 f5 70 83 ee dd
289355 BLEMesh_PvnrDataInputCallback - Node Address Assigned = 1
Device is provisioned by provisioner
293710 BLEMesh_PbAdvLinkCloseCb - PB-ADV Link Closed successfully
293710 AppliPrvnNvm_Process - Saving in SubPage[00000078] =
295710 ConfigClient_CompositionDataGet - Config CompositionDataGet Message
315710 ConfigClient_ChkRetries - Retry started
317710 ConfigClient_CompositionDataGet - Config CompositionDataGet Message
337710 ConfigClient_ChkRetries - Retry started
339710 ConfigClient_CompositionDataGet - Config CompositionDataGet Message
359710 ConfigClient_ErrorState - No response from Node
2020-04-29 6:56 AM
Hi,
After the download of the software, to be sure that your device is unporvisioned:
Unprovision the device:
Run the following command for the self provisioning and the self configuration of your provisioner:
atep root
To be sure that your provisioner is correctly provisioned and configured, just press the SW1 button, if the blue LED is on it is OK, if not unprovisions the device and run again the command atep root.
Now you can run a scan for the unprovisioned devices, with the command:
atep scan
UUID addresses of the unporvisioned devices are displayed as following:
Device-0 -> F81D4FAE7DEC4B53A154F6FB0726E1C0
To provision and configure the device run the command:
atep prvn-0 2
Where:
Parameter 0 is the displayed index of the device
Parameter 2 is the unicast address you want to associates to the provisioned node (1 is used for the provisioner Node)
After running this command, many lines are displayed on the terminal, till the following one:
38281 Appli_ConfigClient_ConfigureNode - **Node is configured**.
Best regards.
2020-05-12 4:29 AM
Hello,
There is the new cube version 1.7.0 but it seems that does not resolve any issue with Mesh and FLASH access.
2020-05-12 5:17 AM
Hello,
Your are right there is no change concerning MESH and FLASH access in this new release.
The trouble you have faced with the ENABLE_PROVISIONER_FEATURE will be solved in the next release.
Did you test the BLE_MeshLightingProvisioner with the DYNAMIC_PROVISIONER defined (as set by default in the mesh_cfg_usr.h file) ?
Best regards.
2020-05-12 10:31 PM
Hello,
I write the post 14 days ago, please see above. I tested Dynamic provisioner and every time I got "No response from Node". Please see the included log.
Best Regards
2023-10-05 11:25 AM
Hello lukasz2,
I'm with the same problem! Did you manage to solve it? Thank you