2024-04-18 03:04 AM
Hello,
We're wondering about the Next_State_Systime field in the end_of_radio_activity events - what kind of time unit is used for it, and how to make a use of it on application side.
Long story short, we'd like to avoid some noise sensible operations in our system while some RF activity - typically an advertisement - is going on. We're struggling to find some data on that subject. We're using a ble full stack on wb55 chips.
BR
2024-05-29 02:47 AM
Hello @grevaillot
The time unit used is the reference for internal time units, it can be System Clock or any other reference Clock.
For the use case. The application uses this information to schedule user activities synchronous to selected radio activities.
More details are available on the AN5270.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.