2024-12-10 03:30 AM
Hi,
I hope everyone is fine.
I have question about Inheritance Certification.
The Thread Group says;
The Thread Group allows certification by inheritance for families of end products that reuse the same Thread system (chip and stack) and the same use cases.
When appropriate stack libraries and SOC or module used End Device Certification can certifiable by Inheritance.
Our company does not have any Thread or Matter-certified products, but if we use ST's certified module and stack library, can we obtain Thread certification for an end device we develop?
Can we use the certification by inheritance feature when using ST's modules?
We want to use a Matter-enabled module and a certified stack binary in our projects; however, we will design a PCB using this module.
We would like to confirm whether soldering components onto the PCB with the module or chip would invalidate the certification by inheritance.
We would greatly appreciate your support with your experience and knowledge.
2024-12-11 05:10 AM
Hello,
yes, you can get the Thread certification by inheritance. But for Matter certification itself, the process is different - there is an option similar to inheritance, but it is related to each individual device type (so light, switch...) and possible cluster configuration. ST does not have such certification at the moment, so it is up to the customer (apart from the applications which are publicly available in the X-CUBE-MATTER package). We can help with pre-certification tests (making sure the device pass cluster functional tests) but the customer needs to apply for membership in CSA and officially pass the tests.
2024-12-11 05:18 AM
Hi,
Thank you for reply.
I have little bit knowledge about Matter certification processes. But, before Matter certification the device's network layer must be certify. At this situation we want to use both Thread and Bluetooth. I just wonder what if we use ST's matter certified module and SDK, Must we still test the device.
2024-12-11 07:44 AM
Hello,
yes, that's what I was trying to say. Maybe it is not clear.
You need to use the M0 stack binary (otherwise, the WB5M cannot operate in general) - this binary manages the network layer. And it is certified as such. It has BLE 5.2 certification and Thread MTD certification. You do not need to do testing of the device.
But you need to provide your own BLE and Thread certifications when you want to apply for Matter certification. You can use ST BLE certification as described here https://wiki.st.com/stm32mcu/wiki/Connectivity:Certification_guideline#Qualification_workspace_process_flow . And you can apply for Inheritance certification for the Thread part. This will be the input to step 6 of the diagram you linked above.
And if you are asking about the product testing in step 5, then this concerns the Matter application layer, which you need to do.