cancel
Showing results for 
Search instead for 
Did you mean: 

1.8V VDDA-Vref Voltage

Makif
Associate

Hello,

 

I have a custom STM32WB55 board and for custom purposes, I want to use VDDA=1.8 V and Vref=1.8 V from same Reference IC. According to datasheet, I can decrease VDDA from 3.3 V to as low as 1.62 V but I just wanted to make sure that it won't cause any problem in terms of VDDA supplied analog circuits etc.

 

Best Regards,

Mehmet.

1 REPLY 1
AScha.3
Chief III

Hi,

from ds:

AScha3_0-1719243075180.png

AScha3_1-1719243120659.png

So at 1,8V you cannot use vrefbuf and no USB .

 

 

If you feel a post has answered your question, please click "Accept as Solution".