2024-01-24 12:54 AM - edited 2024-01-24 12:57 AM
TouchGFX 4.23.1 is now out.
Please follow this link to download it.
4.23.1 Release details:
Release date: January 22nd, 2024
New TouchGFX Designer Features:
Bugfixes in TouchGFX Designer:
New TouchGFX Core Features:
Bugfixes in TouchGFX Core:
Deprecated TouchGFX Core Features:
4.23.0 Release details:
Release date: December 5th, 2023
New TouchGFX Designer Features:
Bugfixes in TouchGFX Designer:
New TouchGFX Core Features:
Bugfixes in TouchGFX Core:
Deprecated TouchGFX Core Features:
Note : TouchGFX Designer 4.23.1 MUST be used with STM32CubeMX 6.10.0 or above (link to download STM32CubeMX).
Attention : If X-CUBE-TOUCHGFX 4.23.1 is not available in STM32CubeMX software yet, please navigate to "Help > Manage embedded software packages > STMicroelectronics > X-CUBE-TOUCHGFX". Then click on "From Local ..." and navigate to the x-cube-touchgfx-4-23-1.zip file to install the new pack inside STM32CubeMX.
Please also check our Known Issues article.
Enjoy this new version ! :)
2024-02-13 01:15 PM
It was said in [this thread](https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/change-scrollwheel-s-content-dynamicaly/m-p/636119#M36039) 4 years ago that there may be a more dynamic implementation of the Scroll Wheel container. Is that something that's still on the radar?
2024-02-21 12:13 AM
I have one problem on TOUCH GFX 4.23.1 and Cube.MX 6.10.0.
I created a STM32F746G_DISCO project with GFX, and generate codes without any modifying.
Next, open STM32F746G_DISCO.ioc with Cube.MX, found following warning.
I searched new X-CUBE-TOUCHGFX package, but latest version in Cube.MX is 4.23.0.
How can I clear this waring?
2024-02-25 09:40 PM
Scalable image does not work in external flash section. The image is not shown on TFT. When i select the Internal flash section, the image is shown on TFT. Or please share us if there are any solution about this problem.
Please fix this problem.
2024-03-03 11:18 PM - edited 2024-03-03 11:19 PM
Here the exact same problem. Downloaded the latest version of CubeMx (6.10) and cannot find TouchGFX 4.23.1
How can this be solved?
2024-03-04 12:26 AM
I found a way to clear this warning, are following steps correct?
Source codes in Middlewares/ST/touchgfx/frameworks/... have following header, and including TouchGFX 4.23.1 is completed with successfuly.
/******************************************************************************
* Copyright (c) 2018(-2024) STMicroelectronics.
* All rights reserved.
*
* This file is part of the TouchGFX 4.23.1 distribution.
*
* This software is licensed under terms that can be found in the LICENSE file in
* the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
*******************************************************************************/
However, when re-opening .ioc files with Cube.MX 6.10.0, I had same warning and the icon of X-CUBE-TOUCHGFX is 'can not edit' state:
2024-03-04 09:54 AM
Hello
Check the initial message of this thread:
Attention : If X-CUBE-TOUCHGFX 4.23.1 is not available in STM32CubeMX software yet, please navigate to "Help > Manage embedded software packages > STMicroelectronics > X-CUBE-TOUCHGFX". Then click on "From Local ..." and navigate to the x-cube-touchgfx-4-23-1.zip file to install the new pack inside STM32CubeMX.
So you must manually install the latest TouchGFX version to the CubeMX. Also here discussed about same problem
https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/can-t-open-ioc-the-cmsis-pack/td-p/635622
hope this helps.
Br JTP
2024-03-04 05:45 PM
Hi JTP,
Thank you for your reply.
I tried your suggestion, and installed GFX 4.23.1 to Cube.MX successfully.
Thanks!!