2023-09-09 10:02 AM
I have been working on a project for many months now with TouchGFX v4.20. I was modifying some of the text strings I had defined in TouchGFX Designer and now the texts/TextKeysAndLanguages.hpp is no longer being generated.
When trying to start the simulator I see that it says something about an unexpected character (see below output). This is halting any work I can do with TouchGFX anybody ever experience this??
Run Simulator
Generate
Done
Generate Assets
make -f simulator/gcc/Makefile assets -j8
Reading ./application.config
Unexpected character at -~
Cleaning generated files from generated/texts and generated/fonts.
Solved! Go to Solution.
2023-09-09 1:01 PM
I guess something got corrupted somehow, I was able to go back to work I saved 3 days ago and start there. Everything builds fine again. Was able to incorporate everything I had done over the past 3 days and still works fine so I guess all is well. Not sure how the TouchGFX project got corrupted but it did.
2023-09-09 10:27 AM
Why no try next releases ?
2023-09-09 11:20 AM
I thought about it but get scared upgrading tools in the middle of a project. didn't see a way to update designer from the application, do I need to do a fresh install for a new release?
2023-09-09 1:01 PM
I guess something got corrupted somehow, I was able to go back to work I saved 3 days ago and start there. Everything builds fine again. Was able to incorporate everything I had done over the past 3 days and still works fine so I guess all is well. Not sure how the TouchGFX project got corrupted but it did.