cancel
Showing results for 
Search instead for 
Did you mean: 

Screen aspect ratio is not right after changing display

ihsanoglu
Senior

I changed the 4.3" 480*272 display on the stm32f746-disco board.

The new display is a 7" 800*480. I modified the resolution from code and also from TouchGFX project.

Everything is working fine. However the screens are displayed like if they are pressed from top and bottom.

To explain more. A prefect circle on the designer is displayed as an oval shape on the display.

Please see the images attached. Notice how the circle turns into an oval when displayed on the screen.

0690X00000AQxbhQAD.png0690X00000AQxfjQAD.png

I need to solve this issue. Is this addressable by code or its a display problem?

This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7
ihsanoglu
Senior

The aspect ratio of the pixels on the display is not 1:1. The pixels are not perfect squares, they are shaped as rectangles. Is there any mechanism in TouchGFX to handle this issue?

ihsanoglu
Senior

Hello could you please look into this ? @Martin KJELDSEN​ 

Martin KJELDSEN
Chief III

Hi @Abdullah İhsanoğlu​,

If your pixels are rectangular, then maybe you do not have the resolution you thought you did? (Along the Y-axis, it seems). Wouldn't this be solved by simply adjusting your Y resolution?

But if your pixels were indeed rectangular on the y axis, then your circles should also be skewed, in my eyes. Are you sure?

/Martin

Hello martin,

This is the resolution mentioned in the datasheet, and actually wheneever I try to decrease the resolution. The image is not getting stretched , only cropped ( missing pixels going black).

Also when increasing the resolution, The pixels beyond the limit are not being displayed. They are beyond the boundary of the display.

So you're saying that you can actually solve this by lowering the resolution to compensate for the "length" of your pixels. It's a bit strange to me because, in my eyes, TouchGFX would need to render differently (A pixel in the designer is smaller than it is on the display for these types of displays and your assets would also have to be different - And yet, the output looks normal.

/Martin

Sorry , no I am not saying that. I am saying the exact opposite.

I just purchased a new display with square pixels. Apparently there is no mechanism in TouchGFX nor in LTDC to componsate for such skewed pixels

matasondas222
Associate

Hello,

I stumbled upon the same issue as the OP.

I created basic TouchGFX GUI with startup screen that uses image (company logo, PNG) and a round progress bar.

You can see the aspect ration problem just by looking at it, we even measured the actual dimensions of the 'round' progress circle with a scale. The actual dimensions: X=21mm Y=19mm. Then I added another TGFX object, a circle (filled, in the picture) to check whether the issue stays (it does, the circle render behavior is the same as for images)

 

We use 7" 480x800 RGB888 panel, type WF70GTIAGDNT0 (Link: Datasheet [PDF] ) where they admit the physical pixel (subpixel) size is not 1:1 width vs. height so I assume this is the same issue as the OP had. We use the STM32H735DK board.

Is there anything to do with this issue on the software level? I didn't find any rendering correction methods in TouchGFX