2022-10-11 7:23 AM
Hi every one. I am using STM32-F401RE, 2x16 LCD with I2C integrate, i connect SCL-SDA-Vcc and GND each other (board and LCD), i tried to make scann program to know adress of LCD in this way:
#include "main.h"
#include "stdio.h"
I2C_HandleTypeDef hi2c1;
UART_HandleTypeDef huart1;
uint8_t Buffer[25] = {0};
uint8_t Space[] = " - ";
uint8_t StartMSG[] = "Starting I2C Scanning: \r\n";
uint8_t EndMSG[] = "Done! \r\n\r\n";
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_I2C1_Init(void);
static void MX_USART1_UART_Init(void);
int main(void)
{
uint8_t i = 0, ret;
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_I2C1_Init();
MX_USART1_UART_Init();
HAL_Delay(1000);
/*-[ I2C Bus Scanning ]-*/
HAL_UART_Transmit(&huart1, StartMSG, sizeof(StartMSG), 10000);
for(i=1; i<128; i++)
{
ret = HAL_I2C_IsDeviceReady(&hi2c1, (uint16_t)(i<<1), 3, 5);
if (ret != HAL_OK) /* No ACK Received At That Address */
{
HAL_UART_Transmit(&huart1, Space, sizeof(Space), 10000);
}
else if(ret == HAL_OK)
{
sprintf(Buffer, "0x%X", i);
HAL_UART_Transmit(&huart1, Buffer, sizeof(Buffer), 10000);
}
}
HAL_UART_Transmit(&huart1, EndMSG, sizeof(EndMSG), 10000);
/*--[ Scanning Done ]--*/
while (1)
{
}
}
but no adress i saw. If i use LCD with Arduino Mega board i am able to see the 0x27 adress of LCD. I used also all the pins avaiable on F401RE board for SCL and SDA comunication but never i see the adress of LCD.
Have some one idea how i can get it(adress of LCD)?
2022-10-19 12:55 PM
good evening, i am not able to see any letter with my system: F401RE Nucleo board and 2x16 LCD with I2C integrate but, i am able to see some things ( some letter and example) if connect LCD with arduino. Can some one show me small program to be able also to see one word in this system built: F401RE and LCD? Maybe i have to change brand and buy some other board from other brand/vendor.
2022-10-19 1:21 PM
>>2x16 LCD
That's a bit generic, what specific make/model are we talking about here? Got a link to the part you purchased?
Arduino Mega, that's a 5V board, sure you have the thing powered correctly? Pull-ups?
It's ALL the other code where the magic really happens, configures the pins, peripherals, clocks, etc.
No detail of anything in the code provided, Cube hides it.
2022-10-21 11:18 AM
Hi, I bought the F401RE Nucleo board on Amazon, I used it for several project and no issue to here. When i tried to connect thos boaard to 2x16 LCD with I2C drive integrated to LCD, i wasn't able to send any letter from board to LCD. The lcd work because i used it on arduino and i see on lcd some letter like : hello word. I create a progect in CUBE IDE, left the standard configuration, i wrote this code in main:
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_I2C1_Init();
/* USER CODE BEGIN 2 */
lcd_init ();
lcd_send_string ("HELLO WORLD");
HAL_Delay(1000);
lcd_put_cur(1, 0);
lcd_send_string("from CTECH");
HAL_Delay(2000);
lcd_clear ();
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
I add two library, this:
First libray:
/** Put this in the src folder **/
#include "i2c-lcd.h"
extern I2C_HandleTypeDef hi2c1; // change your handler here accordingly
#define SLAVE_ADDRESS_LCD 0x4E // change this according to ur setup
void lcd_send_cmd (char cmd)
{
char data_u, data_l;
uint8_t data_t[4];
data_u = (cmd&0xf0);
data_l = ((cmd<<4)&0xf0);
data_t[0] = data_u|0x0C; //en=1, rs=0
data_t[1] = data_u|0x08; //en=0, rs=0
data_t[2] = data_l|0x0C; //en=1, rs=0
data_t[3] = data_l|0x08; //en=0, rs=0
HAL_I2C_Master_Transmit (&hi2c1, SLAVE_ADDRESS_LCD,(uint8_t *) data_t, 4, 100);
}
void lcd_send_data (char data)
{
char data_u, data_l;
uint8_t data_t[4];
data_u = (data&0xf0);
data_l = ((data<<4)&0xf0);
data_t[0] = data_u|0x0D; //en=1, rs=0
data_t[1] = data_u|0x09; //en=0, rs=0
data_t[2] = data_l|0x0D; //en=1, rs=0
data_t[3] = data_l|0x09; //en=0, rs=0
HAL_I2C_Master_Transmit (&hi2c1, SLAVE_ADDRESS_LCD,(uint8_t *) data_t, 4, 100);
}
void lcd_clear (void)
{
lcd_send_cmd (0x80);
for (int i=0; i<70; i++)
{
lcd_send_data (' ');
}
}
void lcd_put_cur(int row, int col)
{
switch (row)
{
case 0:
col |= 0x80;
break;
case 1:
col |= 0xC0;
break;
}
lcd_send_cmd (col);
}
void lcd_init (void)
{
// 4 bit initialisation
HAL_Delay(50); // wait for >40ms
lcd_send_cmd (0x30);
HAL_Delay(5); // wait for >4.1ms
lcd_send_cmd (0x30);
HAL_Delay(1); // wait for >100us
lcd_send_cmd (0x30);
HAL_Delay(10);
lcd_send_cmd (0x20); // 4bit mode
HAL_Delay(10);
// dislay initialisation
lcd_send_cmd (0x28); // Function set --> DL=0 (4 bit mode), N = 1 (2 line display) F = 0 (5x8 characters)
HAL_Delay(1);
lcd_send_cmd (0x08); //Display on/off control --> D=0,C=0, B=0 ---> display off
HAL_Delay(1);
lcd_send_cmd (0x01); // clear display
HAL_Delay(1);
HAL_Delay(1);
lcd_send_cmd (0x06); //Entry mode set --> I/D = 1 (increment cursor) & S = 0 (no shift)
HAL_Delay(1);
lcd_send_cmd (0x0C); //Display on/off control --> D = 1, C and B = 0. (Cursor and blink, last two bits)
}
void lcd_send_string (char *str)
{
while (*str) lcd_send_data (*str++);
}
Second library:
#include "stm32f4xx_hal.h"
void lcd_init (void); // initialize lcd
void lcd_send_cmd (char cmd); // send command to the lcd
void lcd_send_data (char data); // send data to the lcd
void lcd_send_string (char *str); // send string to the lcd
void lcd_put_cur(int row, int col); // put cursor at the entered position row (0 or 1), col (0-15);
void lcd_clear (void);
but i see no letter on LCD.
I supply the LCD with 5 V of the board. I didn't found any tutorial on web using this F401RE Nucleo with LCD but only other kind of STM32 board. Maybe this board have some issue in this kind of application?
I tried to use all possible SDA/SCA pins canghing the IC2, IC3 but nothing working. Attached some pictures of my project. I used arduino mega and there working.
If some one can help me i can send the entire project.
2022-10-21 11:20 AM
2022-10-21 1:01 PM
The question was with regard to the make/model of "16x2" display.
Guessing it's using an I2C IO Expander to drive as a 4-bit controller.
Any of the I2C commands error?
Show any of the pin initialization code?
2022-10-21 1:07 PM
Do you check the return code from I2C functions? Are you sure that the LCD responds?
Here you can find helping hands to get started.
2022-10-21 3:50 PM
Likely the one here
https://controllerstech.com/i2c-lcd-in-stm32/
Illustrate your wiring. Prior post only has a single picture, not pictures
2022-10-21 11:52 PM
Hi, no error , nothing. Here i post the LCD model. I saw 10 times the video you send me: https://controllerstech.com/i2c-lcd-in-stm32/ because i used the information on that video to create and to add library and code.
I attach three picture (model of LCD that is the same used on the video) and configuration end wiring.
Here all the programm where can see the pin inizialization:
#include "main.h"
#include "i2c-lcd.h"
I2C_HandleTypeDef hi2c1;
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_I2C1_Init(void);
int row=0;
int col=0;
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_I2C1_Init();
lcd_init ();
lcd_send_string ("HELLO WORLD");
HAL_Delay(1000);
lcd_put_cur(1, 0);
lcd_send_string("from CTECH");
HAL_Delay(2000);
lcd_clear ();
while (1)
{
}
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 16;
RCC_OscInitStruct.PLL.PLLN = 336;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
RCC_OscInitStruct.PLL.PLLQ = 7;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{
Error_Handler();
}
}
static void MX_I2C1_Init(void)
{
hi2c1.Instance = I2C1;
hi2c1.Init.ClockSpeed = 100000;
hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
hi2c1.Init.OwnAddress1 = 0;
hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c1.Init.OwnAddress2 = 0;
hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if (HAL_I2C_Init(&hi2c1) != HAL_OK)
{
Error_Handler();
}
}
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET);
GPIO_InitStruct.Pin = B1_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct);
GPIO_InitStruct.Pin = LD2_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(LD2_GPIO_Port, &GPIO_InitStruct);
}
void Error_Handler(void)
{
__disable_irq();
while (1)
{
}
}
#ifdef USE_FULL_ASSERT
void assert_failed(uint8_t *file, uint32_t line)
{
}
#endif /* USE_FULL_ASSERT */
2022-10-21 11:55 PM
no video related the retur code you talk