2022-06-16 04:03 PM
I've been having an odd issue where if I add any widgets into a custom container the i2c ADC devices stop responding. I've isolated it to the point where I can just add any default widget into the container and then run target in the designer to see the issue. Once I go back and delete that widget all functions resume working.
When I go to debug the issue in cubeide the issue is not reproducible. The code compiled within the IDE works as intended with or without the added widgets.
2022-06-24 02:25 AM
Hello Physwm2501,
Could you give more information about your configuration please ?
Are you using a TouchGFX Board Setup or did you start your project from scratch?
/Osman