2026-05-12 10:50 PM - last edited on 2026-05-18 12:59 AM by mƎALLEm
I am trying to interface STM32U5G7VJT6 with MT25QL128A using OCTOSPI1 in Quad SPI mode, but I still cannot store/run TouchGFX assets from external flash memory.
Current configuration:
Screenshot attached.
Could someone please check if I missed any important configuration like memory-mapped mode, linker settings, TouchGFX asset location, BSP/init sequence, or MT25QL128A command setup?
2026-05-13 12:53 AM
Hello @Furkan2;
--> Screenshot attached.
Could you please add the screenshot.
Can you do read and write operations on the external flash memory?
I recommend you to look at AN5050 section "7 OCTOSPI application examples" may help you.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-05-13 3:39 AM
Thank you for your response.
I have attached the OCTOSPI1 configuration screenshots and related settings.
Currently, I am not able to MT25QL128A external flash memory, so TouchGFX assets are also not working from external flash.
I will also check AN5050 section 7 as suggested.
2026-05-18 12:32 AM
Hello @Furkan2;
Thank you for these details.
Is the problem solved when displaying TouchGFX and read/write operations from external buffer?
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-05-18 12:37 AM
Dear Kaouthar,
Thank you for your support.
The external flash read/write operation is working correctly now, and the external buffer is accessible in memory-mapped mode.
However, the TouchGFX display issue is not fully solved yet. The LCD no longer stays completely white, but the image rendering is unstable/blurry and sometimes becomes white again during TouchGFX execution.
Currently:
External OSPI flash read/write: Working
Memory-mapped mode: Working
LTDC initialization: Working
Framebuffer in SRAM: Configured
TouchGFX rendering: Still unstable
I am currently checking LTDC timing and framebuffer configuration.
Thank you.
2026-05-18 12:48 AM
Hello @Furkan2;
I advise you to look at Introduction to LCD-TFT display controller (LTDC) for STM32 MCUs - Application note and How to set up the LTDC peripheral to interface with the display panel ATM0500D27-CT from AZ Displays may help you.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-05-18 3:10 AM
Thank you for your response.
I will review the application note “Introduction to LCD-TFT display controller (LTDC) for STM32 MCUs” and also check the example for interfacing the ATM0500D27-CT display panel.
Currently, the external OSPI flash memory is working correctly in memory-mapped mode, and read/write access is successful. However, the TouchGFX display is still showing a white/blurry screen issue.
I will verify the LTDC timing and framebuffer configuration again based on the provided references.
Thank you for your supports