2023-01-04 1:23 AM
Hello,
I've bought the Riverdi RVT70HSSNWC00-B STM32H7 embedded display.
But i'm unable to flash my app to the board.
Here are the log from touchGFX :
-------------------------------------------------------------------
STM32CubeProgrammer v2.11.0
-------------------------------------------------------------------
ST-LINK SN : 39FF6D064E56363921500143
ST-LINK FW : V2J40S7
Board : --
Voltage : 3.28V
SWD freq : 4000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x450
Revision ID : Rev V
Error: Database: There's no active configuration for this device. All the 8 configurations are disabled!
Error: Database: There's no active configuration for this device. All the 8 configurations are disabled!
Device name : STM32H7xx
Flash size : 63 KBytes (default)
Device type : MCU
Device CPU : Cortex-M7
BL Version : --
Warning: Write address is ignored for hex, Srec, s19 and elf files
Memory Programming ...
Opening and parsing file: intflash.hex
File : intflash.hex
Size : 243.99 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Error: Unable to get core ID
Erasing external memory sector 0
Error: failed to erase memory
Error: failed to erase memory
-------------------------------------------------------------------
STM32CubeProgrammer v2.11.0
-------------------------------------------------------------------
ST-LINK SN : 39FF6D064E56363921500143
ST-LINK FW : V2J40S7
Board : --
Voltage : 3.09V
SWD freq : 4000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x450
Revision ID : Rev V
Error: Database: There's no active configuration for this device. All the 8 configurations are disabled!
Error: Database: There's no active configuration for this device. All the 8 configurations are disabled!
Device name : STM32H7xx
Flash size : 63 KBytes (default)
Device type : MCU
Device CPU : Cortex-M7
BL Version : --
Memory Programming ...
Opening and parsing file: extflash.bin
Error: The file extflash.bin is empty
Hard reset is performed
make[2]: Leaving directory 'c:/TouchGFXProjects/MyApplication'
make[1]: Leaving directory 'C:/TouchGFXProjects/MyApplication/gcc'
Done
And here are the log from STM32CubeProgrammer:
I'm a very beginner workins with STM32 and don't finda lot about these.
Can someone help me please ?
Solved! Go to Solution.
2023-01-04 7:12 AM
I've found the solution. I used the ST-LINK/V2 Isolated version between the boardand my PC but it needs the non-isolated version of it to works. I took one on a nucleo board and it works weel.
Thanks for your answers @MM..1 !
2023-01-04 2:49 AM
Try change Connect mode to Under reset
2023-01-04 4:30 AM
I'm facing the same issue. And now I've a new error above "Error: Database..." :
"Error : Unable to get core ID"
2023-01-04 5:23 AM
Try latest 2.12 version prog or an older.
2023-01-04 7:12 AM
I've found the solution. I used the ST-LINK/V2 Isolated version between the boardand my PC but it needs the non-isolated version of it to works. I took one on a nucleo board and it works weel.
Thanks for your answers @MM..1 !
2024-03-29 1:43 PM
I also started the development with an embedded Riverdi STM32 display. In the example from TouchGFX, all peripherals are configured on one M7 core.
Are you using two cores in your development? Did you manage to configure the core-M4?