2021-03-15 7:28 AM
Hi
When switching between screens fast, my UI always ends up freezing. Debugging reveals that it waits forever, waiting for the frame buffer semaphore.
Here is the call stack:
Inspecting other running tasks shows nothing wrong. Only the graphics task should touch the frame buffer semaphore, right? So it should never deadlock?
Environment:
2021-04-12 2:37 AM
Hi @Martin KJELDSEN
So, here's what we are using :
Once stuck :
Here's the DMA2D registers :
2021-04-12 4:00 AM
Thanks for the detailed info!
2021-04-15 1:37 AM
Hi @Martin KJELDSEN,
Any update on that ? Let me know if you need more information or test I can do.
Thanks
2021-04-23 2:05 AM
Hi @Martin KJELDSEN,
Still no updates on this issue ? It's been more than a month after opening this issue, and it is not progressing. Is there another channel for support than this forum ?
Thanks,
Tony
2021-04-27 12:01 AM
Hey Tony, sorry man. Let me add @Romain DIELEMAN to this thread. We're a bit short on support effort these days. You're constantly on my mind (along with a few others).
You say you're using Atollic - Did you hack together this project yourself? What are the priorities for the threads and interrupts? We don't officially support the old Atollic IDE.
If this is automatically generated i'm not expecting this to be the issue. But it does look like there's a race condition- Just to be clear - Can you share your project? I think i'll need to look at some code at this point
/Martin
2021-04-29 2:55 AM
Hi @Martin KJELDSEN
So we're using Atollic because we started the project when it was the begining of the CubeIDE and the full integration of TouchGFX in CubeMX. Then, we kept TouchGFX up to date.
For source sharing, can we switch to email to discuss that ?
Thanks,
Tony
2021-05-03 12:58 AM
Sure, let's do that. Pretty sure my email is in my profile.
2021-06-08 12:37 AM
Just an update for everyone following the thread:
From the stack trace it is clear that touchgfx gets stuck while drawing a series of glyphs. This is something we've fixed in more recent versions of TouchGFX. I'm following this avenue of thought with OP by email.
/Martin
2021-06-21 12:33 AM
Hi @Martin KJELDSEN : We have a similar issue in our display.
Can you please provide some details about the solution for this problem ?
You say that that touchgfx gets stuck while drawing a series of glyps and it is being fixed in more recent versions. Can you please say in which version this is being fixed ?
2021-06-21 12:44 AM
Which version are you using? There was a bug, once, but we're talking way back, where lockFrameBuffer() would cause a deadlock if a glyph was the last thing to be transferred by DMA2D.
/Martin