‎2025-05-17 8:04 AM
Hello everyone,
I'm facing an issue with jumping from my application to the bootloader on an STM32H747 microcontroller. I'm using a 7-inch Riverdi display and have developed graphical interfaces using TouchGFX. My application, which I've built using only the M7 core (disabling the M4 core) and FreeRTOS for task management and graphics, has its main file structured as man1.c attached.I've also created a bootloader program with the following structure: The bootloader works perfectly when the STM32H747xx_FLASH.ld file contains the following instruction:
Assolutamente! Ecco la traduzione del tuo post in inglese, adatta per un forum tecnico come quello di STM:
Subject: Trouble Jumping to Bootloader from Application on STM32H747 with Riverdi Display and TouchGFX
Hello everyone,
I'm facing an issue with jumping from my application to the bootloader on an STM32H747 microcontroller. I'm using a 7-inch Riverdi display and have developed graphical interfaces using TouchGFX. My application, which I've built using only the M7 core (disabling the M4 core) and FreeRTOS for task management and graphics, has its main file structured as follows:
I've also created a bootloader program with the following structure:
The bootloader works perfectly when the STM32H747xx_FLASH.ld file contains the following instruction:
MEMORY
{
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
/*FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 1024K*/ /* Memory is divided. Actual start is 0x08000000 and actual length is 2048K */
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 250K
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
SDRAM (xrw) : ORIGIN = 0xD0000000, LENGTH = 4M
SDRAM2 (xrw) : ORIGIN = 0xD0400000, LENGTH = 4M
}
However, when I try to jump to the bootloader from my application using a jump_to_bootloader() function, the jump to the bootloader fails. This is code snipet:
I've made to the .ld files of both the application and the bootloader.
// Application .ld
/* Memories definition */
MEMORY
{
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
/*FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 1024K*/ /* Memory is divided. Actual start is 0x08000000 and actual length is 2048K */
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 724K
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
QUADSPI (r) : ORIGIN = 0x90000000, LENGTH = 64M
SDRAM (xrw) : ORIGIN = 0xD0000000, LENGTH = 4M
SDRAM2 (xrw) : ORIGIN = 0xD0400000, LENGTH = 4M
}
// Bootloader.ld
/* Memories definition */
MEMORY
{
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
/*FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 1024K*/ /* Memory is divided. Actual start is 0x08000000 and actual length is 2048K */
FLASH (rx) : ORIGIN = 0x08B500000, LENGTH = 250K
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
SDRAM (xrw) : ORIGIN = 0xD0000000, LENGTH = 4M
SDRAM2 (xrw) : ORIGIN = 0xD0400000, LENGTH = 4M
}
Could someone please advise on what modifications I need to make in both the application and the bootloader code to successfully jump to the bootloader? Is there something I'm missing in the process?How may I had to manage all peripherals?
Thank you in advance for your help!
Solved! Go to Solution.
‎2025-06-03 4:25 AM
In basic reply deinit isnt required, but for clean visual some steps as off backlight , stop refresh display is ok.
Some peripherals for example RTC isnt reset with NVIC reset , but i mean you dont use it.
Then simply create noinit variable marker and set it to right value before reset ...
‎2025-06-05 5:51 AM
Hi everyone!
After a lot of trial and error, I finally solved my STM32 dual-application setup issue. I created two projects:
A bootloader, which starts at address 0x08000000
An application, located at 0x08020000
they have these .ld files
Bootloader .ld (128KB at start of Flash):
MEMORY
{
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 128K
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
}
and .ld file for the second project.
MEMORY
{
FLASH (rx) : ORIGIN = 0x08020000, LENGTH = 896K
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
QUADSPI (r) : ORIGIN = 0x90000000, LENGTH = 64M
SDRAM (xrw) : ORIGIN = 0xD0000000, LENGTH = 4M
SDRAM2 (xrw) : ORIGIN = 0xD0400000, LENGTH = 4M
}
In the main.c file of bootloader I use this function
typedef void (*pFunction)(void);
static void JumpToApplication(void)
{
__disable_irq(); // Disable all interrupts
HAL_RCC_DeInit(); // Reset clock configuration
HAL_DeInit(); // Deinit peripherals
SysTick->CTRL = 0; // Disable SysTick if running
__set_MSP(*(__IO uint32_t*)0x08020000); // Set new MSP from app vector table
SCB->VTOR = 0x08020000; // Point VTOR to new app
uint32_t JumpAddr = *(__IO uint32_t*)(0x08020000 + 4); // Reset_Handler address
pFunction Jump = (pFunction)JumpAddr;
__enable_irq(); // Re-enable interrupts if needed
Jump(); // Execute the jump
NVIC_SystemReset(); // If jump fails, reset
}
Everything now works perfectly. The bootloader initializes, then jumps to the second application at 0x0802000 without issues.
Big thanks to everyone who offered support and tips during this process — your help made it happen!