2025-05-03 5:39 AM
Hello,
this error really drives me crazy. When trying to flash the programm from the ToughGFX App or CubeIDE the external Memory can't be erased. I use the recommended CubeMXVersion of 6.14 and have the latest CubeProgrammer and CubeIDE with STM32Cube FW_U5 V1.7.0. The whole ToughGFX log is attached. Thanks in advance!
These are the following errors that are occurring:
TouchGFX:
Erasing memory corresponding to sector 0:
Erasing external memory sector 0
Error: failed to erase memory
gcc/include/flash_sections_int_ext.mk:5: recipe for target '_extflash_' failed
make[1]: *** [_extflash_] Error 1
../gcc/Makefile:52: recipe for target 'flash' failed
make: *** [flash] Error 2
Failed
Failed
CubeIDE:
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
\STM32CubeIDE\\Debug\\STM32U575ZI-NUCLEO-AZ2.elf
Error message from debugger back end:
Error finishing flash operation
Error finishing flash operation