2024-08-23 7:25 AM
Hello,
I saw couple questions being asked back in 2019, 2020 and 2022 on this topic but with a hope that situation may have changed, I am asking to get some clarification.
I have a requirement to run the TouchGFX on a Linux based HMI.
Priority would be to run on Yocto Linux running on iMX6 board, or else run on any other HMI that has Ubuntu as the host OS.
Using the designer I can get simulator.exe that can run very well on windows, however if I can please get to know if any support available to run this on Linux based systems that would be great help.
Hardware is not STM based board. Would like to use TouchGFX Designer as HMI development tool.
Is it possible? Thank you for your support and consideration.
Solved! Go to Solution.
2024-08-23 7:29 AM - edited 2024-08-23 8:25 AM
Hello,
You cannot use TouchGFX library on other platform other than STM32 MCUs and it's protected internally against this kind of use case.
2024-08-23 7:29 AM - edited 2024-08-23 8:25 AM
Hello,
You cannot use TouchGFX library on other platform other than STM32 MCUs and it's protected internally against this kind of use case.