2020-11-08 7:54 PM
Dear ST Team,
I'm doing a project about: display LCD (DSI Video mode) with TouchGFX. I have example TouchGFX DSI Adapted CMD mode, but can't find out example for DSI video mode.
Please give me some idea!!!
Thanks
Solved! Go to Solution.
2020-11-09 1:10 AM
Hi, please select "Parallel RGB (LTDC)" from the TouchGFX Generator. It should work for DSI video mode. Our current Application templates for DSI are configured to Adapted command mode and as such have handlers to transfer bits of the framebuffer through dsi, manually. But for video mode, you don't need those, just the LTDC handler.
2020-11-09 1:10 AM
Hi, please select "Parallel RGB (LTDC)" from the TouchGFX Generator. It should work for DSI video mode. Our current Application templates for DSI are configured to Adapted command mode and as such have handlers to transfer bits of the framebuffer through dsi, manually. But for video mode, you don't need those, just the LTDC handler.
2020-11-10 8:09 PM
Hi Martin,
Thank you for your reply. It works well !!
2020-11-11 2:34 AM
Great :) I now realize there's no mention of this anywhere, so i'll add it to the documentation and perhaps change the option from inside Generator to indicate that it also works for DSI Video Mode.