cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX with Dropbox not working

Ricko
Senior III

Hi,

TouchGFX does not like spaces in the path. I just wanted to check a couple of things please:

 

1) that is referring to the/my project path only, is that correct?

 

2) For those of you who use Dropbox, the Dropbox PC folder name cannot be changed and it always contains the team or person name + a space + "Dropbox". So it seems you cannot have your projects stored on Dropbox. And I would really need to have them there. Are there any workaround? How do you do it?

 

Thank you :)

 

1 ACCEPTED SOLUTION
2 REPLIES 2

Hi @MM..1 

thank you for the links. The first seems to solve it.:thumbs_up:

 

The second I don't know how it can work, as mentioned in my OP, accoding to Dropbox tech support (I have a business account) the name cannot be changed, it always has to have that structure I mentioned. That was according to two different people at DB tech support during two different calls.

 

Why ask here? Because it is a TouchGFX related issue and question and other than calling DB, where else would I ask (especially not knowing about the idea of network mapping).

 

Thank you again for the reply :)