2025-03-04 3:33 AM
if (!textClock.isMoveAnimationRunning()) .. fails
after following the tutorial i receive ..
Compile
make -f simulator/gcc/Makefile -j8
Reading ./application.config
Reading ./target.config
Compiling gui/src/screen2_screen/Screen2View.cpp
Compiling generated/texts/src/TypedTextDatabase.cpp
gui/src/screen2_screen/Screen2View.cpp: In member function 'virtual void Screen2View::handleTickEvent()':
gui/src/screen2_screen/Screen2View.cpp:63:20: error: 'class touchgfx::TextArea' has no member named 'isMoveAnimationRunning'
if (!textClock.isMoveAnimationRunning())
^~~~~~~~~~~~~~~~~~~~~~
generated/simulator/gcc/Makefile:196: recipe for target 'build/MINGW32_NT-6.2/gui/src/screen2_screen/Screen2View.o' failed
make[2]: *** [build/MINGW32_NT-6.2/gui/src/screen2_screen/Screen2View.o] Error 1
make[2]: *** Waiting for unfinished jobs....
make[1]: *** [generate_assets] Error 2
generated/simulator/gcc/Makefile:155: recipe for target 'generate_assets' failed
simulator/gcc/Makefile:32: recipe for target 'all' failed
make: *** [all] Error 2
Failed
Failed
i've added #include <touchgfx/mixins/MoveAnimator.hpp> to screen2view.cpp as well ..
I'm new to this so unsure what or where the problem is ?
i've read the documentation and .. "isMoveAnimationRunning" can be found ..
anyone shed any light please ...
2025-03-04 7:29 AM
Thank you , it seams to work other than the minutes are going up as seconds .. i'm more bothered about it compiling
:) . i have got it set up for my dev kit though maybe that's it ..
Regards
John
2025-03-05 2:59 AM - edited 2025-03-05 2:59 AM
I got it to build and simulate.
Just uncomment these two lines in Screen2View.hpp:
//Unicode::UnicodeChar textClockBuffer1[TEXTCLOCKBUFFER1_SIZE];
//Unicode::UnicodeChar textClockBuffer2[TEXTCLOCKBUFFER2_SIZE];
//TextArea textClock; // Ensure this matches your UI component type
Screen2View inherits from Screen2ViewBase, which inherits from Screen2Presenter. The textClock is already in the base class:
touchgfx::Draggable< touchgfx::ClickListener< touchgfx::FadeAnimator< touchgfx::MoveAnimator< touchgfx::TextAreaWithTwoWildcards > > > > textClock;
As you can see it is no longer simply a TextArea class.