cancel
Showing results for 
Search instead for 
Did you mean: 

Touchgfx timer hardware (TIM5) in ScreenView.cpp ??

MRebo.1
Associate II

Hi, I would like that use a callback of timer (programmed with 10ms) to override the "ScreenView::handleTickEvent()" function, because this function has interrupt in ~14ms.

I managed to create the function and link the cpp and C files, but I couldn't use C++ functions (about graph..) in the timer callback that I created, there is an error like "was not declared in this scope" in which when I use it in the "handleTickEvent" function there is no error. Why is this happening?

Here is the .c file:

#include <gui/main_screen/MainView.hpp>
#include <math.h>
#include <stdlib.h>
 
extern "C" void CallbackTim5();
 
int slide_value = 0;
 
int xlabel_0 = 10;
int xlabel_1 = 11;
int xlabel_2 = 12;
int xlabel_3 = 13;
int xlabel_4 = 14;
int xlabel_5 = 15;
int xlabel_6 = 16;
int xlabel_7 = 17;
int xlabel_8 = 18;
int xlabel_9 = 19;
int xlabel_10 = 20;
 
int contDataPoint=0;
int msCounter=0;
 //here dont works
void CallbackTim5(){
	msCounter++;
 
	// Insert each second tick
	if (msCounter % 2 == 0)
	{
		// Insert "random" points along a sine wave
		graph_control.addDataPoint(10);
		graph_response.addDataPoint(20);
		graph_setpoint.addDataPoint(slide_value);
 
		contDataPoint++;
		if(contDataPoint >= 300){
 
			contDataPoint = 0;
			if((xlabel_0 >= 300) && (xlabel_0 < 1000)){
				Unicode::snprintf(xLabelGraph1Buffer, 147,
				"%d   %d   %d   %d   %d   %d   %d   %d   %d   %d   %d",
				xlabel_0, xlabel_1, xlabel_2, xlabel_3, xlabel_4, xlabel_5,
				xlabel_6, xlabel_7, xlabel_8, xlabel_9, xlabel_10);
 
				xLabelGraph1.invalidate();
 
				Unicode::snprintf(xLabelGraph2Buffer, 147,
				"%d   %d   %d   %d   %d   %d   %d   %d   %d   %d   %d",
				xlabel_0, xlabel_1, xlabel_2, xlabel_3, xlabel_4, xlabel_5,
				xlabel_6, xlabel_7, xlabel_8, xlabel_9, xlabel_10);
			}
			else if(xlabel_0 >= 1000){
				Unicode::snprintf(xLabelGraph1Buffer, 147,
				"%d%d%d%d%d%d%d%d%d%d%d",
				xlabel_0, xlabel_1, xlabel_2, xlabel_3, xlabel_4, xlabel_5,
				xlabel_6, xlabel_7, xlabel_8, xlabel_9, xlabel_10);
 
				xLabelGraph1.invalidate();
 
				Unicode::snprintf(xLabelGraph2Buffer, 147,
				"%d%d%d%d%d%d%d%d%d%d%d",
				xlabel_0, xlabel_1, xlabel_2, xlabel_3, xlabel_4, xlabel_5,
				xlabel_6, xlabel_7, xlabel_8, xlabel_9, xlabel_10);
			}
			else{
				Unicode::snprintf(xLabelGraph1Buffer, 147,
				"%d      %d       %d      %d      %d      %d      %d      %d      %d      %d      %d",
				xlabel_0, xlabel_1, xlabel_2, xlabel_3, xlabel_4, xlabel_5,
				xlabel_6, xlabel_7, xlabel_8, xlabel_9, xlabel_10);
 
				xLabelGraph1.invalidate();
 
				Unicode::snprintf(xLabelGraph2Buffer, 147,
				"%d      %d       %d      %d      %d      %d      %d      %d      %d      %d      %d",
				xlabel_0, xlabel_1, xlabel_2, xlabel_3, xlabel_4, xlabel_5,
				xlabel_6, xlabel_7, xlabel_8, xlabel_9, xlabel_10);
			}
 
 
			xLabelGraph2.invalidate();
 
			xlabel_0 += 10;
			xlabel_1 += 10;
			xlabel_2 += 10;
			xlabel_3 += 10;
			xlabel_4 += 10;
			xlabel_5 += 10;
			xlabel_6 += 10;
			xlabel_7 += 10;
			xlabel_8 += 10;
			xlabel_9 += 10;
			xlabel_10 += 10;
		}
	}
}
 
MainView::MainView()
{
    tickCounter = 0;
}
 
void MainView::setupScreen()
{
    MainViewBase::setupScreen();
 
    // Initialize graph range with default slider value at start up
    sliderValueChanged(sliderSetpoint.getValue());
}
 
void MainView::tearDownScreen()
{
    MainViewBase::tearDownScreen();
}
 
//here works
void MainView::handleTickEvent()
{
//    tickCounter++;
//
//    // Insert each second tick
//    if (tickCounter % 2 == 0)
//    {
//        // Insert "random" points along a sine wave
//        graph_control.addDataPoint(10);
//        graph_response.addDataPoint(20);
//        graph_setpoint.addDataPoint(slide_value);
//
//        contDataPoint++;
//        if(contDataPoint >= 300){
//
//            contDataPoint = 0;
//            if((xlabel_0 >= 300) && (xlabel_0 < 1000)){
//                Unicode::snprintf(xLabelGraph1Buffer, 147,
//                "%d   %d   %d   %d   %d   %d   %d   %d   %d   %d   %d",
//                xlabel_0, xlabel_1, xlabel_2, xlabel_3, xlabel_4, xlabel_5,
//                xlabel_6, xlabel_7, xlabel_8, xlabel_9, xlabel_10);
//
//                xLabelGraph1.invalidate();
//
//                Unicode::snprintf(xLabelGraph2Buffer, 147,
//                "%d   %d   %d   %d   %d   %d   %d   %d   %d   %d   %d",
//                xlabel_0, xlabel_1, xlabel_2, xlabel_3, xlabel_4, xlabel_5,
//                xlabel_6, xlabel_7, xlabel_8, xlabel_9, xlabel_10);
//            }
//            else if(xlabel_0 >= 1000){
//                Unicode::snprintf(xLabelGraph1Buffer, 147,
//                "%d%d%d%d%d%d%d%d%d%d%d",
//                xlabel_0, xlabel_1, xlabel_2, xlabel_3, xlabel_4, xlabel_5,
//                xlabel_6, xlabel_7, xlabel_8, xlabel_9, xlabel_10);
//
//                xLabelGraph1.invalidate();
//
//                Unicode::snprintf(xLabelGraph2Buffer, 147,
//                "%d%d%d%d%d%d%d%d%d%d%d",
//                xlabel_0, xlabel_1, xlabel_2, xlabel_3, xlabel_4, xlabel_5,
//                xlabel_6, xlabel_7, xlabel_8, xlabel_9, xlabel_10);
//            }
//            else{
//                Unicode::snprintf(xLabelGraph1Buffer, 147,
//                "%d      %d       %d      %d      %d      %d      %d      %d      %d      %d      %d",
//                xlabel_0, xlabel_1, xlabel_2, xlabel_3, xlabel_4, xlabel_5,
//                xlabel_6, xlabel_7, xlabel_8, xlabel_9, xlabel_10);
//
//                xLabelGraph1.invalidate();
//
//                Unicode::snprintf(xLabelGraph2Buffer, 147,
//                "%d      %d       %d      %d      %d      %d      %d      %d      %d      %d      %d",
//                xlabel_0, xlabel_1, xlabel_2, xlabel_3, xlabel_4, xlabel_5,
//                xlabel_6, xlabel_7, xlabel_8, xlabel_9, xlabel_10);
//            }
//
//
//            xLabelGraph2.invalidate();
//
//            xlabel_0 += 10;
//            xlabel_1 += 10;
//            xlabel_2 += 10;
//            xlabel_3 += 10;
//            xlabel_4 += 10;
//            xlabel_5 += 10;
//            xlabel_6 += 10;
//            xlabel_7 += 10;
//            xlabel_8 += 10;
//            xlabel_9 += 10;
//            xlabel_10 += 10;
//        }
//    }
}
 
void MainView::sliderValueChanged(int value)
{
	slide_value = value;
}
 
void MainView::resetButtonEvent(){
 
}
 
void MainView::setButtonEvent(){
 
}
 
void MainView::autoButtonEvent(){
 
}

 Error:

0693W00000BdUpzQAF.png 

Without Error:

0693W00000BdUqJQAV.png 

2 REPLIES 2
MM..1
Chief II

How display config you use _? LTDC ? TickEvent is based on refresh rate on LCD for example 60Hz ... around 16ms , then when your display support and you need 10ms setup it to 100Hz frame refresh...

Jnevi.1
Senior

you cannot access a member of MainView like graph_control from a c function.

your callback must be a member of your view if you want to use this concept