2019-08-29 1:27 AM
Hello
I'm working with the stm32h750 eval board and touchgfx, my GUI is ready, but now i need to conect to some hardware (relay, sensors etc). i usually work with keil, but touchgfx not generating keil project and i lost hope it will before my dead-end; so i moved to IAR, which is generated, but not working, seems to me all options for the generated project are wrong, after many attempt (some random, some *** grano salis) i was able to compile a project, but still not able to load it into board (IAR starts to load project, and keeps going forever, no error, nothing, and i waited 40 min to see if it will eventually unstuck and load the code)
any advice/guide/working example to load touchGFX project from IAR?
Thanks
2019-08-29 1:31 AM
Hi @Zui,
Sorry you're having so much trouble. First off, can you show me some logs or give me some explanation of what isnt working in IAR? Second, you _can not_ program external flash from IAR. You need to use ST-Link/STCubeProgrammer.
/Martin
2019-08-30 1:45 AM
so i will never be able to debug my code?
2019-08-30 3:47 AM
Yes you can. You just cannot program the QSPI with IAR (which seems to be the error you're getting). Use ST-Link or STMCubeProgrammer and just use IAR to program the internal flash.
/Martin