2024-05-14 8:56 PM
Hi,
I'm using a custom H7 board, with QSPI + 16-bit SDRAM, and using RTOS.
However I run into an issue where there's glitching in my gauge in TouchGFX (see attached video...)
TouchGFX is using double buffer, also animationStorage:
setFrameBufferStartAddresses((void*)0xC0000000, (void*)0xC0177000, (void*)0xC0400000);
A few points:
- I'm able to read/write to QSPI & SDRAM correctly
- Static images appear correctly
- Glitch also appears on the whole screen during transition from one image to another
MPU:
static void MPU_Config(void)
{
MPU_Region_InitTypeDef MPU_InitStruct;
/* Disable the MPU */
HAL_MPU_Disable();
/* Configure the MPU attributes for region 0 */
/* Configure the MPU attributes for SDRAM to normal memory*/
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER0;
MPU_InitStruct.BaseAddress = 0xC0000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_256MB;
MPU_InitStruct.SubRegionDisable = 0x0;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Configure the MPU attributes for region 1 */
/* Configure the MPU attributes for the frontbuffer to normal memory*/
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER1;
MPU_InitStruct.BaseAddress = 0xC0000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_1MB;
MPU_InitStruct.SubRegionDisable = 0x0;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Configure the MPU attributes for region 2 */
/* Configure the MPU attributes for the backbuffer to normal memory*/
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER2;
MPU_InitStruct.BaseAddress = 0xC0200000;
MPU_InitStruct.Size = MPU_REGION_SIZE_1MB;
MPU_InitStruct.SubRegionDisable = 0x0;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Configure the MPU attributes for region 3 */
/* Configure the MPU attributes for Quad-SPI area to strongly ordered memory*/
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER3;
MPU_InitStruct.BaseAddress = 0x90000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_64MB;
MPU_InitStruct.SubRegionDisable = 0x0;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.AccessPermission = MPU_REGION_NO_ACCESS;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Configure the MPU attributes for region 4 */
/* Configure the MPU attributes for QSPI memory to normal memory*/
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER4;
MPU_InitStruct.BaseAddress = 0x90000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_16MB;
MPU_InitStruct.SubRegionDisable = 0x0;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.AccessPermission = MPU_REGION_PRIV_RO;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Enable the MPU */
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
}
Clock Configurations:
- System: 480 MHz
- FMC : 150 MHz
- LTDC : 20.15 MHz
- QUADSPI : 150 MHz
My LTDC & TouchGFX Configurations:
Can anyone please tell me why this happens? Thanks..
Solved! Go to Solution.
2024-10-07 8:19 AM
Im not H7 expert, but i mean PNG is not supported for TGFX direct store and decode in hw. Instead TGFX decode png in generate process and compile choiced image format in flash. Try explain what you try do? SW png decoders exist , but is slow...
2024-10-09 3:04 AM
Hey @wlynn777,
Have you set your display to portrait in the TouchGFX Designer?
Could you please (just for testing purposes) set your Display Type to RGB888 instead of ARGB888 in the LTDC settings? Pixel Format should be also set to RGB888. After applying these changes, the Framebuffer Pixel Format in TouchGFX Generator parameters should be changed to RGB888
2024-10-10 9:14 PM
Yes, the display orientation is already portrait.
Have tried this too, no difference..
2024-10-10 9:33 PM
2024-10-11 2:14 AM
Are you sure your display have sync-porch 4 8 8 ?
Next source maybe pcb design, but primary check mmory real values ? Exist here lines or not.
Next issue i see in your screenshots Active width 832 , this is not normal when display is 800, but exist special configs with this shift...
LTDC clock you set for lower framerate as 60Hz ...
2024-12-06 10:58 PM
Okay, I got it to work but without the DMA2D, and I switched to RGB565.
I also did these, which removed the glitches and artifacts:
- Initialized FMC_NBL0 and FMC_NBL1 pins (crucial, as it turns out...)
- Set MPU of the SDRAM to:
MPU_InitStruct.BaseAddress = 0xC0000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_32MB;
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;- Disabling the DCache also helped during troubleshooting.
Thanks to everyone who has helped answer.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.