cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX Engine Stop / Resume to Save Power

YSN
Senior
  1. Is there any way to stop touchgfx (with DMA2D) engine and resume back after notification.
  2. Stop and Resume of Touchgfx task is not a solution as the DMA streaming is running in the background. Pls confirm ?
  3. Start / Stop / Resume the touchgfx engine to save the power as FMC/SDRAM/QSPI will also have to stall with option? Is it possible ?

1 REPLY 1
KDubo
Associate II

Hello, did you ever get a resolution on this? The only way I can get TouchGFX to resume after MCU is in STOP mode is to delete / create the TouchGFX task, which is not ideal.