cancel
Showing results for 
Search instead for 
Did you mean: 

Touchgfx Designer is not opening in the computer.

MPath.4
Associate II

 last time also this problem was occured so I installed it again after that it run for some days now again the problem has occured.

 When I open Touchgfx one msg come

Sorry - something unexpected has happened which caused an error to occur in the Designer.

For more information, see the log file located at: C:\Users\Kaushal\AppData\Roaming\TouchGFX-4.21.3\TouchGFXDesigner.log

Please someone help to give the solution of it.

25 REPLIES 25
MPath.4
Associate II
 
Yoann KLEIN
ST Employee

Hello,

This file looks empty or erroneous, did you modify it before sharing it ?

/Yoann

Yoann KLEIN
ST Software Developer | TouchGFX
MPath.4
Associate II

No I didn't I send it to you once again

MPath.4
Associate II
 
MPath.4
Associate II

This is another one.

posted a file.

MPath.4
Associate II

It happened yesterday in the older version also when I generated code in stm32cubemx

Yoann KLEIN
ST Employee

When you open this file in a text editor, what do you see ?

/Yoann

Yoann KLEIN
ST Software Developer | TouchGFX

Actually the touchgfx doesn't open so I can't open any of these files.

But I didn't modify it because I can't do it.

I mean, when you right click on it and open it with Notepad.

/Yoann

Yoann KLEIN
ST Software Developer | TouchGFX

It is showing nul in last 3 to 4 projects just check this one