2024-08-11 10:45 AM
Hello all,
I'll be starting a project in TouchGFX designer from an existing template, say STM32F469I DISCO. How does the code generation by the TouchGFX designer and CubeMX interact? Say when I add an UI element and regenerate the code in designer, does it respect the hardware changes done in CubeMX? Or, if I do some changes in CubeMX (for example, add some GPIOs or an UART), does CubeMX generation preserve all TouchGFX code?
Is there an order I need to be aware of or can I mix both? What about custom code I added, will it be overwritten by TouchGFX designer code generation? I work a lot with CubeMX so I know how the system with the tags work.
What about CubeMX not used standalone, but from within STM32CubeIDE?
Thanks! Martin