2020-04-28 03:14 AM
Hello, I and using Touchgfx in my project. I want to implement below.
1) During run time , I want to to turn off complete screen.
2) During run time , I want to change complete screen.
3) I want to generate QR code dynamically and also want to clear it sometimes during run time. I got github link and added those files in my project. Still I am not sure how to call it. You have mentioned to call qrCode.setXY(0,0) , qrCode.setQRCode(&code), qrCode.setScale(4) , add(qrCode) methods but I am unable to find it.
Can any one please help ?
Solved! Go to Solution.
2020-04-28 10:20 PM
Actually i generated touchgfx from ST32MXCube so if I am not sure which task are you taking about related to touchgfx? Can you tell name so i can check ?
Also i didn't find any this related to thing in ST32MXCube .
2020-04-28 11:36 PM
I checked in code but didn't find any task related to same. Please suggest.
2020-04-29 01:03 AM
Look in the FreeRTOS configuration in CubeMX to find the stack size.
2020-04-29 01:09 AM
Already checked but didn't find it. Below are the images from cubemx.
2020-04-29 06:08 AM
@Martin KJELDSEN hi, did u get the chance to check ?
2020-04-29 07:06 AM
"Tasks and queues"
2020-04-29 07:26 AM
its already 4096 words.
2020-04-29 08:07 AM
Is this CMSISV1 or V2 ? For V2, that window is actually wrong. It's no longer in words, but in bytes.
2020-04-29 08:09 AM
its CMSIS V1
2020-04-29 08:13 AM
Okay you'll have to do some more debugging then.