2021-12-13 01:22 PM
I have an application where there is a potential for lots of text. It would be nice to break up the next into a bulleted list or a numbered list. Is there a clever way to do this with the Touchgfx framework?
I think making typed text values for each block will be too tedious for the amount of text I will be working with. The only other option I can think of is creating an image of the formatted text and using that.
Thanks.
Solved! Go to Solution.
2021-12-21 07:00 AM
It turns out that if you use bulleted text in the Excel spreadsheet, that bullets will carry over into the text generated for the application:
2021-12-18 10:46 AM
Maybe nobody understand without example, try show one or two onscreen texts
2021-12-21 07:00 AM
It turns out that if you use bulleted text in the Excel spreadsheet, that bullets will carry over into the text generated for the application: