cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX and DCMI together

eng23
Senior

Hi,

I'm adding camera to my custom board with TouchGFX using DCMI.

I have doubts on how to put video camera in framebuffer used by TouchGFX..

I've created 2 framebufferes in LTDC and the first is used by Touch. I don't know if I use the second framebuffer to camera and show the second in LCD or I use the same framebuffer for both. How I leave TouchGFX using framebuffer...

Thanks.

11 REPLIES 11

Hi Martin,

Yes, I've found this on H7 family and it was the reason that I ask about H7 TouchGFX support.

I have a short time for this project so at this moment I won't change to H7 family, but when I have more time I need to do this.

Thanks for this advices!

Regards