Skip to main content
Associate II
May 8, 2025
Solved

TouchGFX 4.25.0 update + OPEN AMP on STM32H7

  • May 8, 2025
  • 2 replies
  • 523 views

OS: Windows 10

STM32CubeIDE version: 1.18.1

Board: STM32H757XIH6

My project was made in TouchGFX 4.23.2. The project uses both cores on the board, they communicate with openamp. After updating to TouchGFX 4.25.0 and generating from ioc with the TGFX 4.25.0 generator. Openamp on the M4 core goes to error handler everytime. Openamp on M7 seems to be working. 

If I run the original software, not updated to TGFX 4.25.0 everything works as expected.

This is the openamp code on M4:

 int status;
	MAILBOX_Init();

	if(MX_OPENAMP_Init(RPMSG_REMOTE, NULL) != HAL_OK){
		Error_Handler();
	}

	status = OPENAMP_create_endpoint(&rp_endpoint, RPMSG_SERVICE_NAME, RPMSG_ADDR_ANY, rpmsg_recv_callback, NULL);
	if(status < 0){

		Error_Handler();
	}
	receive_message();

 

This is the openamp code in a task on M7:

 

	int status;
	MAILBOX_Init();
	rpmsg_init_ept(&rp_endpoint, RPMSG_CHAN_NAME, RPMSG_ADDR_ANY, RPMSG_ADDR_ANY, NULL, NULL);

	if(MX_OPENAMP_Init(RPMSG_MASTER, new_service_cb) != HAL_OK)
	{
		Error_Handler();
	}

	OPENAMP_Wait_EndPointready(&rp_endpoint);


	status = OPENAMP_send(&rp_endpoint, &received_data, sizeof(received_data));

 

 

This topic has been closed for replies.
Best answer by mƎALLEm

Hello,

Look at these threads: thread 1 , thread 2 as it could be the origin of your issue.

2 replies

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
May 8, 2025

Hello,

Look at these threads: thread 1 , thread 2 as it could be the origin of your issue.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Associate II
May 10, 2025

@Jakicaa 
Maybe you can reference this video. TouchGFX + OpenAMP example