cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX 4.17.0 ,"you are not connected to internet" error is showing

SV
Associate

Hi,

when TouchGFX 4.17.0 is opened I'm getting an error stating no internet connectivity even though my laptop is connected to internet . also in the selection of boards I'm not getting any board option .

thanks and regards

sinduja

60 REPLIES 60

Hi,

The server is not down at the moment. Could you try to open an internet browser and re open TouchGFX Designer again ?

/Romain

Hi,

  • internet browser open at start of TouchGfx Designer: error 409
  • internet browser closed at start of TouchGfx Designer: error 407

Please see messages from log file below.

Thanks.

-----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

Messages from log file (with internet browser open) => error 409:

2021-09-14 07:44:39,835 [1] INFO TouchGFXDesigner.App: Logging configured

2021-09-14 07:44:40,777 [1] ERROR Utils.WebHandling.WebHandler: The remote server returned an error: (409) Conflict.

System.Net.WebException: The remote server returned an error: (409) Conflict.

  at System.Net.HttpWebRequest.GetResponse()

  at System.Net.WebClient.GetWebResponse(WebRequest request)

  at System.Net.WebClient.OpenRead(Uri address)

  at Utils.WebHandling.WebHandler.RequestWithStringResponse(Uri uri)

2021-09-14 07:44:41,496 [1] INFO TouchGFXDesigner.Main.MainWindow: Application started

2021-09-14 07:44:41,497 [1] INFO TouchGFXDesigner.Main.MainWindow: Username: ***

2021-09-14 07:44:41,497 [1] INFO TouchGFXDesigner.Main.MainWindow: Designer version: 4.17.0

2021-09-14 07:44:41,497 [1] INFO TouchGFXDesigner.Main.MainWindow: Designer installation path: C:\TouchGFX\4.17.0\designer

2021-09-14 07:44:41,497 [1] INFO TouchGFXDesigner.Main.MainWindow: Windows version: Microsoft Windows NT 10.0.19042.0

2021-09-14 07:44:41,497 [1] INFO TouchGFXDesigner.Main.MainWindow: Current culture: de-DE

2021-09-14 07:44:41,502 [1] INFO TouchGFXDesigner.Main.MainWindow: Current culture time seperator: :

2021-09-14 07:44:41,502 [1] INFO TouchGFXDesigner.Main.MainWindow: Current culture date seperator: .

2021-09-14 07:44:41,504 [1] INFO TouchGFXDesigner.Main.MainWindow: Installed .NET version(s): v2.0.50727 2.0.50727.4927 SP2v3.0 3.0.30729.4926 SP2v3.5 3.5.30729.4926 SP1v4 (Client 4.8.04084 Full 4.8.04084 ) v4.0 (Client 4.0.0.0 )  

2021-09-14 07:44:45,705 [17] ERROR Utils.WebHandling.WebHandler: The remote server returned an error: (409) Conflict.

System.Net.WebException: The remote server returned an error: (409) Conflict.

  at System.Net.HttpWebRequest.GetResponse()

  at Utils.WebHandling.ServerRequest.GetResponse()

  at Utils.WebHandling.WebHandler.RequestHeadStatusResponse(Uri uri)

-----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

Messages from log file (with internet browser closed) => error 407:

2021-09-14 07:39:52,556 [1] INFO TouchGFXDesigner.App: Logging configured

2021-09-14 07:39:53,473 [1] ERROR Utils.WebHandling.WebHandler: The remote server returned an error: (407) Proxy Authentication Required.

System.Net.WebException: The remote server returned an error: (407) Proxy Authentication Required.

  at System.Net.HttpWebRequest.GetResponse()

  at System.Net.WebClient.GetWebResponse(WebRequest request)

  at System.Net.WebClient.OpenRead(Uri address)

  at Utils.WebHandling.WebHandler.RequestWithStringResponse(Uri uri)

2021-09-14 07:39:54,183 [1] INFO TouchGFXDesigner.Main.MainWindow: Application started

2021-09-14 07:39:54,185 [1] INFO TouchGFXDesigner.Main.MainWindow: Username: ***

2021-09-14 07:39:54,185 [1] INFO TouchGFXDesigner.Main.MainWindow: Designer version: 4.17.0

2021-09-14 07:39:54,185 [1] INFO TouchGFXDesigner.Main.MainWindow: Designer installation path: C:\TouchGFX\4.17.0\designer

2021-09-14 07:39:54,185 [1] INFO TouchGFXDesigner.Main.MainWindow: Windows version: Microsoft Windows NT 10.0.19042.0

2021-09-14 07:39:54,185 [1] INFO TouchGFXDesigner.Main.MainWindow: Current culture: de-DE

2021-09-14 07:39:54,191 [1] INFO TouchGFXDesigner.Main.MainWindow: Current culture time seperator: :

2021-09-14 07:39:54,192 [1] INFO TouchGFXDesigner.Main.MainWindow: Current culture date seperator: .

2021-09-14 07:39:54,194 [1] INFO TouchGFXDesigner.Main.MainWindow: Installed .NET version(s): v2.0.50727 2.0.50727.4927 SP2v3.0 3.0.30729.4926 SP2v3.5 3.5.30729.4926 SP1v4 (Client 4.8.04084 Full 4.8.04084 ) v4.0 (Client 4.0.0.0 )  

Yes, I can access this image.

Hi,

any idea what causes that error 409?

Thanks.

Unfortunately not. Could you try using TouchGFX Designer 4.16.1 ? I suppose you are using a proxy server ? When you open TouchGFX 4.16.1 do you get a pop up message at startup asking for id/password?

/Romain

Yes, with version 4.16.1 a popup message appears for proxy login and internet connection then works successfully.

Unfortunately, in version 4.16.1 I cannot find an example configured for STM32H735G-DK evaluation board like in version 4.17.0.

Is such an example also available for 4.16.1?

Thanks.

Ok so it is a big issue that will be fixed. In the meantime I will share the tpa for the STM32H735G-DK. You need to unzip it and add it to your C:\TouchGFX\4.17.0\app\packages folder and then open TouchGFX Designer again. Like you said this TBS is not available in TouchGFX 4.16.1

/Romain

Hi,

can you please also provide the tpa-file for STM32G071-NUCLEO-DEMO with 240x320 LCD?

I tried to copy the file from TouchGFX Designer 4.16.1 to 4.17.0, but STM32G071-NUCLEO-DEMO is not shown in the boards list under "create new".

Thanks.

If it is the demo you are looking for and not the TBS for the STM32G071-nucleo board, then it should be under the "Board Specific Demo" tab in the "Demos" section. But I guess you will face the same issue downloading it. I'll try to find it :thumbs_up:.

​

/Romain