cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX�?서 사용하는 �?�미지 형�? 문�?�?

PKunK.1
Associate III

0693W00000CzeCRQAZ.pngThe project created by stm32f469 is set to RGB565. Asking if 24Bit Foramt can be used when using images in TouchGFX.

As far as I know, RGB565 is 16Bit and 24Bit is in RGB888 format.

Can I use a 24Bit image?

If the setting is RGB565, can you tell me if I must use a 16Bit image?

1 ACCEPTED SOLUTION

Accepted Solutions
Romain DIELEMAN
ST Employee

Hi,

You can use a 24bit image but it will be transformed into 16bit image by the DMA2D in your project.

/Romain

View solution in original post

1 REPLY 1
Romain DIELEMAN
ST Employee

Hi,

You can use a 24bit image but it will be transformed into 16bit image by the DMA2D in your project.

/Romain