Touch Panel 7inch can't run with TouchGFX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-03-29 7:16 AM
I have make a customize Board using STM32F746 base on STM32F746-Disco board. but i'm using TFT 7inch with capacitor touch panel using IC FT5425.
I have tested with touch panel base on example in BSP folder of STM32Cube. it run normaly. that mean FT5246 Touch on myboard same FT5336 Touch on STM32F746-Disco.
But when i combine it in the touchGFX it can't run, although i edit and fit Touch size = 800x480
You can see my issue at this link: https://www.youtube.com/watch?v=tTGpPzTiMxs&t=1s or attached file.
I hope some expect can help me solve this problem, this i project very important for me.
Thanks and best regards.
- Labels:
-
STM32F7 Series
-
TouchGFX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-03-30 2:46 AM
Hi,
This looks more like a global congestion of the memory bus to me than only a touch panel issue.
Indeed the touch panel seems to work, but the refresh of the framebuffer does not seem correct.
Could you give a detail description of your setup ?
800x480 definition display, but in 16 or 24 bits ? I would suggest 16 bits for this definition to reduce the memory bandwidth if your display supports it.
How many frame buffers ? 1, 2, 3 (I guess so for the slide animation)
Where are they located ? In same memory bank ? Did you check the following application note on performances AN4861 ?
Best regards,
Nicolas